cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Communication Failure Between External I2C Master and CY8CPLC10 - KBA216056

Anonymous
Not applicable

Communication Failure Between External I2C Master and CY8CPLC10 - KBA216056

Version: **

Translation - Japanese: 外部I2CマスターとCY8CPLC10間の通信障害 - KBA216056 - Community Translated (JA)

Question:

The CY8CPLC10 device does not seem to respond to the I2C commands sent by an external I2C master. However, it responds correctly when using CY3240 I2C-USB Bridge and PLC control Panel as the I2C master. What could be a possible reason for this issue?

Answer:

The minimum required "Bus Free Time Between a STOP and START Condition" for the I2C interface to CY8CPLC10 is 500 µs (as can be found in CY8CPLC10 device datasheet).

A violation of this specification has seen to be a common cause for communication failure between external master controllers and CY8CPLC10. Please verify if this specification is adhered to in your external master code.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Aug 18, 2016 11:30 PM
Updated by:
Anonymous
 
Contributors