cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Clock input to analog CT (continuous time) blocks in PSoC1?

PriyadeepK_01
Employee

Clock input to analog CT (continuous time) blocks in PSoC1?

Question: Why do CT (continuous time) blocks have clock input in PSoC1?

 

Answer:

The continuous time blocks have a latch for the comparator bus output. This latch synchronizes the output with the column clock i.e. the output of the comparator changes only during the clock edge (selected by the Cphase bit in the ACBxxCR2 register). Note that the latch may also be configured as transparent (i.e. the output changes immediately as the input is changed) by setting the CLatch bit in the ACBxxCR2 register to 0.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Feb 25, 2011 01:59 PM
Updated by:
 
Contributors