cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

CY7C66113 be used as a dual device

Anonymous
Not applicable

CY7C66113 be used as a dual device

Question: Can the hub part, CY7C66113 be used as a dual device (2 keyboard  for example) hub connected to a host. Is this possible without the need for a hardware "wedge" circuit or a special driver?

 

Answer:

No. The only way that  this device allows for two implementations is as a Hub + function, no Function + Function is allowed.

USB does allow for multiple keyboards (in Windows, potential  problems in Mac platform with multiple keyboards)  You would need Two micro's, one to implement each keyboard and USB would take care of noticing the two keyboards seperately on the Host side.

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Jul 05, 2011 02:31 AM
Updated by:
Anonymous
 
Contributors