BUTTON_MODE Bit 7 set to 0 for 56-pin packages of CY7C68300C
Anonymous
Not applicable
Mar 26, 2011
08:42 AM
- Subscribe to RSS Feed
- Mark as New
- Mark as Read
- Bookmark
- Subscribe
- Printer Friendly Page
- Report Inappropriate Content
Mar 26, 2011
08:42 AM
Question: Why should the BUTTON_MODE Bit 7 be set to 0 for the 56-pin packages of CY7C68300C?
Answer:
The ATAPUEN which is enabled or disabled by the BUTTON_MODE Bit 7 is available only in 100 pin package of CY7C68300C. As the 56 pin package does not support this feature, BUTTON_MODE Bit 7 has to be disabled for this package.
Rate this article:
Contributors
-
This widget could not be displayed.Anonymous