Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Alternate pin for SPI slave clock pin in CY8C20xx6

Alternate pin for SPI slave clock pin in CY8C20xx6

Anonymous
Not applicable
Question: How to use the the alternate pin for SPI slave clock pin in CY8C20xx6

 

Answer:

When using SPIS UM in CY8C20xx6 ,by default P1.3 is selected as the slave clock pin. There is an alternate option to use P1.0 as the slave clock by setting the Bit 2, SPICLK_ON_P10 in the register IO_CFG1. We need to change the pin configuration in the pinout window of the designer. Two things need to be done here:

1) Set properties of P1.0:

Name: SPISSCLK (here, the UM is named as SPIS. If it's named as SPIS_1, the name should be set as SPIS_1SCLK)

Select: StdCPU

Drive: Open Drain Low

Interrupt: DisableInt

AnalogMuxBus: Normal

InitialValue: 1

 

2) Change back the properties of P1.3 to its default values:

Name: Port_1_3

Select: StdCPU

Drive: High Z Analog

Interrupt: DisableInt

AnalogMuxBus: Normal

InitialValue: 0

 

Make sure to set the bit SPICLK_ON_P10 in the register IO_CFG1 before calling SPI_Start() API:

IO_CFG1 |= 0x04; 

0 Likes
298 Views
Contributors