cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

Adding a variable to watch windows 2, 3 and 4 in PSoC Creator

Anonymous
Not applicable

Adding a variable to watch windows 2, 3 and 4 in PSoC Creator

Question: How to add a variable to watch window 2, 3 and 4 in PSoC Creator?

 

Answer:

There are two ways to add variable to watch window 2, 3 and 4. First open the watch window you want from debug --> Windows --> Watch. Now in the watch window, under field name you need to type the same of variable you want to add to this watch window. Another way to add variable is to right click on variable and select add watch.(In future version of tool it will be available for all the watch windows)

0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Sep 08, 2010 09:07 AM
Updated by:
Anonymous
 
Contributors