Version: **
The letters U, SV, E, and SE represent the access mode of the register as follows:
Letters |
Description |
U |
Access permitted in User mode 0 or 1 (applicable to write and read). |
SV |
Access permitted in Supervisor mode (applicable to write and read). |
E |
ENDINIT protected write. “E” means a write access is only allowed when ENDINIT is inactive (for a short time window) after a correct ENDINIT password unlock sequence as described in the SCU chapter. |
SE |
Safety ENDINIT protected write. “SE” means a write access is only allowed when safety ENDINIT is inactive (for a short time window) after a correct Safety ENDINIT password unlock sequence as described in the SCU chapter. |
For more details, see the Register access modes section in the user’s manual.