Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

AURIX™ MCU: QSPI pin configuration

AURIX™ MCU: QSPI pin configuration

IFX_Publisher2
Employee
Employee
25 likes received 1000 replies posted First like given

What is QSPI?

 

Queued synchronous peripheral interface (QSPI) functions as master or slave modes. Depending on the mode selected, the pin configuration is as follows:

When the master mode is selected:

 

  • MRSTxA to MRSTxH can be the input for the QSPIx
  • MTSRx is the output of the QSPIx

When the slave mode is selected:

 

  • MTSRxA to MTSRxH can be the input for the QSPIx
  • MRSTx is the output of the QSPIx     

 

For more details, see the "Queued Synchronous Peripheral Interface (QSPI)” section of the user manual.

Note: This KBA applies to the following series of AURIX™ MCUs:

  • AURIX™ TC2xx series
  • AURIX™ TC3xx series

 

 

Community Translation: AURIX™ MCU: QSPIピン設定 – KBA235129

Version: **

370 Views