cancel
Showing results for 
Search instead for 
Did you mean: 

Knowledge Base Articles

ACM mode of FX2LP

Anonymous
Not applicable

ACM mode of FX2LP

Question: Can the CY7C68013A (FX2LP) be programmed to act in CDC/ACM device?

 

Answer:

 

It can be put in CDC-ACM mode but you have to write the descriptors accordingly.The Communication Device Class(CDC) is a device level definition and is used by the host to properly identify a communication device that may present several different types of interfaces.The CDC ACM driver exposes the USB device as a virtual modem or a virtual  COM port to the operating system.For more information on the implementaion refer to AN58764:Implementing a Virtual COM Port in FX2LP
0 Likes
Version history
Revision #:
1 of 1
Last update:
‎Apr 29, 2011 06:52 AM
Updated by:
Anonymous
 
Contributors