Tip / ログイン to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

警告:.LITERAL / .ENDLITERALラベル内の機械命令 - KBA83511 - Community Translated (JA)

警告:.LITERAL / .ENDLITERALラベル内の機械命令 - KBA83511 - Community Translated (JA)

GeethaP_31
Employee
Employee
50 questions asked 10 questions asked 5 questions asked

Community Translated by NoTa_4591161          Version: *A

Translation - English: Warning: Machine Instructions Inside .LITERAL/.ENDLITERAL Labels - KBA83511

質問:

Probable ERROR! Machine instructions inside .LITERAL/.ENDLITERAL will cause problems with Code Compression optimization」とは、PSoC Designerプロジェクトをビルドするときでしょうか?

回答:

これは、ImagecraftコンパイラV7.05以降で追加された警告です。.Literalおよび.EndLiteralディレクティブは、これらのディレクティブ内に配置されたコンテンツを圧縮しないようにコンパイラに指示するために使用されます。一般に、これらのディレクティブは、カスタムデータテーブルをフラッシュに配置する必要がある場合に使用されます。これは、コード圧縮によって変更しないでください。これらのディレクティブ内に機械命令コードが配置されている場合、コードは圧縮されず、ユーザーには上記の警告が通知されます。ユーザーがこれらのディレクティブ内のコードを圧縮しないことを希望する場合、この警告は安全に無視できます。

0 件の賞賛
97 件の閲覧回数
寄稿者