Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

IGBT Forum Discussions

RunBack
IGBT
目前在做T型三电平逆变器项目,横管用的IKWH50N65EH7,竖管用的IKZA75N120CH7,在做双脉冲测试时,由于竖管的dic/dt较大,导致横管的dif/dt达到了-1800A/us,对应的图表里都没有相关的数据,请问如何判断二极管是否处在安全工作区SOA,另外table 5中的Diod... Show More
acong
IGBT

在LTspice软件里面导入AIKQ120N75CP2_L1的spice模型,生成的symbol,是否包含反并联二极管的特性参数?

官网是否有单独的Si diode的spice模型?#spice#

Thangamuthu-N
IGBT

Could you please suggest IGBT driver for FF450R12KT4

1003653144
IGBT
工程师您好,           做实验时IGBT栅极在开关时总是发生震荡,看到贵公司的书中有这样的知识点,如图下 “如图7.3所示”该段话中,为了抑制或衰减振荡,可以用一个小电阻和电容串联。 请问有推介多大的电容和电阻吗?该电容是额外增加的电容Cge吗?     Show More
KRainer
IGBT
Hi everyone, I'm in search of a reliable Thermal Interface Material (TIM) for IGBT modules, specifically in the 900 and 1600 Amp range. Could anyone s... Show More
Translation_Bot
IGBT
Hello, I would like to ask according to the data of FF600R17KF6C_B2 specification. The collector-emitter cutoff current is 5 mA at VCE = 1700 V, VGE =... Show More
YuTa_4942221
IGBT
Please confirm the surface roughness of the heat sink mounted on the 62mm package.AN says ≤10...15μm, but is it correct to understand that it is 10~15... Show More
Gensets
IGBT
We are looking for part numbers or manufacturer of a 4 pin plug to fit on the gate emitter connection of a 62mm igbt package such as FF800R12KE7 Does ... Show More
Slience
IGBT
您好, 关于IGBT单管Input, output and reverse transfer capacitance Cies, Coes and Cres的测试频率,为什么有的是100kHz(IKY140N120CH7),有的是1MHz(IKQ75N120CT2)呢?对于这个频率的选择有什么考究呢... Show More
Slience
IGBT

您好,

关于IGBT模块(FP30R06W1E3)的热阻抗曲线,我看到贵司规格书中只画了RthJH,我该如何得到RthJC的对应关系呢?

Forum Information

IGBT

Infineon’s IGBTs (Discretes and Modules) are available from 600 V to 6500 V with different current ratings and in different topologies targeting almost infinite number of applications. Find support from the community for your next project using products and evaluation boards offered by Infineon.