IGBT Modules

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
iamprt
IGBT Modules

How can I find the details about the auxiliary circuits needed to properly drive IKCM30F60GD?

User22320
IGBT Modules
Select models: FF300R12ME4 and FF300R17ME4. Intend to use the IGBT internal NTC resistor as the overheat protection sampling. What temperature is appr... Show More
User22320
IGBT Modules
Project: Battery Pack Testing System (900kW) Output voltage: 1300~1500V Please recommend suitable IGBT module I need 2500V IGBT module, current: 3... Show More
NXTY_Yoshimura
IGBT Modules
Dear all,Regarding FP50R12N2T4 and FP75R12N2T4, do you have Converter Power Loss Curve , which is the “ AVERAGE FORWARD POWER DISSIPATION “ of attache... Show More
User16691
IGBT Modules
Hello to allI had a problem with an inverter and i did not understand the problem:I have a inverter full bridge, input 125 Vcc and output 230 Vac 60 H... Show More
User21344
IGBT Modules
Hello,We are estimating the costs of an inverter to start a motor that operates for only 5 seconds and then rests for 15 seconds, in the worst case. T... Show More
User20847
IGBT Modules
What is the highest operating temperature of the FS50R07W1E3 chip????150 or 175?
User20724
IGBT Modules
ipw90r340c3用于dcdc全桥电路上,全桥拓扑的输入电压500v左右,一个产品用4个ipw90r340c3,分别为q0500,q0501,q0502,q0503... Show More
User20533
IGBT Modules
Hi, I'm looking for a development KIT to start a project with Easy module F3L15R12W2H3_B27 (3-level) in up to 30A. With included Easy module, drivers,... Show More
User20324
IGBT Modules
What is the relationship between case temperature (or interface temp between the IGBT module and the cooling module) and the overall efficiency of of ... Show More
Top labels