Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Gate Driver ICs Forum Discussions

MaKo_4831421
Level 4
First like given 25 sign-ins 10 replies posted
Level 4

お客様はIRS2109Sから2ED2109S06Fへ置き換えを検討しています。

1.
2ED2109S06Fに関して、INとSDのInternal Pull-up/Pull-downの値を教えて下さい。

2.
2ED2109S06F Datasheetのp4のBlock Diagramでは、SDは+5VにPull-upされています。
この+5VとはVccのことですか?
もし、Vcc=12Vであれば、内部で12VにPull-upされますか?

お手数ですが、ご回答宜しくお願いします。

0 Likes
1 Solution
TakashiM_61
Moderator
Moderator 500 solutions authored 750 replies posted 500 replies posted
Moderator

【回答1】INとSDのInternla Pull-up/down抵抗は同じ値になります。

2ED2109S06F データシートの下記Input bias current Typical 25uA、5Vから200kΩ程度のPull-up/down抵抗が接続されています。

TakashiM_61_0-1660524706527.png

https://www.infineon.com/dgdl/Infineon-2ED2109-4-S06F-J-DataSheet-v02_31-EN.pdf?fileId=5546d4626cb27... 

【回答2】2ED2109S06F DatasheetのBlock Diagram内の+5VはVccではありません。

Vcc=12Vであっても+5Vになります。

View solution in original post

0 Likes
1 Reply
TakashiM_61
Moderator
Moderator 500 solutions authored 750 replies posted 500 replies posted
Moderator

【回答1】INとSDのInternla Pull-up/down抵抗は同じ値になります。

2ED2109S06F データシートの下記Input bias current Typical 25uA、5Vから200kΩ程度のPull-up/down抵抗が接続されています。

TakashiM_61_0-1660524706527.png

https://www.infineon.com/dgdl/Infineon-2ED2109-4-S06F-J-DataSheet-v02_31-EN.pdf?fileId=5546d4626cb27... 

【回答2】2ED2109S06F DatasheetのBlock Diagram内の+5VはVccではありません。

Vcc=12Vであっても+5Vになります。

0 Likes