Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Gate Driver ICs Forum Discussions

Youcef_RZ
Gate Driver ICs
I hope this message finds you well. I am reaching out regarding a couple of questions I have about the datasheet for the IR2109(4)(S). Firstly, I am c... Show More
CVCW
Gate Driver ICs
What power output is the 2EDN7524F FET driver capable of?I need to generate a 1MHz 20V p-p square wave into 50 Ohms. This is a current of just 400mA d... Show More
petbernt
Gate Driver ICs
Hello, I am trying to configure two 1edi2002as devices in a daisy chain configuration for three phases, so six devices in total. I am able to configur... Show More
dtorrese
Gate Driver ICs
I have the following circuit to drive a 3 phase BLDC motor, I'm generating a 20kHz PWM signal for the MOSFETs, however I'm not sure about the correct ... Show More
Engin_TANRIKULU
Gate Driver ICs
Hello, I am using a circuit for motor control. GateDrive is on fire, I think this is a hardware problem. Can you examine the circuit?   Show More
Thai
Gate Driver ICs
Hello, I would like to use the IFX007T for driving a resistive load (~10Ohm). I would like to drive it at 200Hz, how can I calculate the resistor at p... Show More
KOISHI0516
Gate Driver ICs
I am currently using the IRS21084S as a gate driver for a half-bridge inverter, but I am having trouble, so I would like to know about a driver that m... Show More
TJ__
Gate Driver ICs
Hi, The RFE pin is used to enable, fault reporting and programmable fault clear timer, it should only get triggered by either ITRIP OCP event or under... Show More
mgarbuli
Gate Driver ICs
Dear all I am developing a smps full bridge input 48 Vdc, output 200+200Vdc 4800 W, 50 kHz. I want to use the driver IR2110 and in the bridge there ar... Show More
AkUm
Gate Driver ICs
In the data sheet (Page 8), the target pins (HIN, LIN, ITRIP, EN) are listed in the Vin, clamp section. In addition, the internal circuit diagram show... Show More
Forum Information

Gate Driver ICs

Every switch needs a driver – the right driver makes a difference. Find your perfect driver with help from our community on our more than 500 EiceDRIVER™ gate driver IC solutions suitable for any power switch, and any application.