Forums Forum Discussions
Browse the Community
USB
Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.
Wireless Connectivity
Power
Sensors
Memories
Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.
Other Technologies
Discussion forum regarding Other Technologies including Power Management and Clocks topics.
Security & Smart Card
Radio Frequency (RF)
Software
Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .
Applications
Featured Discussions
Hi
I have a general question about the SOA curve provided in the datasheet of MOSFETs.
I have several 48V consumers (DC-Fan, DCDC-Converters) which I would like to switch by MOSFETs instead of relais, as it is now in our application The Vds will be between 42-58V usually. If I look at the SOA of e.g. the IAUA250N08S5N018
am I only allowed to drive around 2A @50Vds? DS also says 35A continuous which confuses me.
My worst case values are 16A @56V, can IAUA250N08S5N018 handle this?
Thank you.
Andy
Show LessHi Infineon Experts:
I want to know for TC3XX series, Is it possible for one GTM_ATOM channel trigger multiple VADC Channels/ VADC Sync Groups?
Thanks for your support in advance.
Show Less请问imotion IMC100可以实现modbus协议通信吗,如果可以,MCE中的flash rom如何读写?
Hello,
We are using TLE4999C8 Hall Sensor, for our application we wanted to implement the Short Serial Message (SSM) feature.
We are able to successfully communicate with TLE4999C8 using SENT interface, however we are not able to verify the 8 bit CRC.
Could you please help us with some sample code to calculate the 8bit CRC for the short serial message format and SPC.
Thank you,
Jannick
Show LessHi All
We have developed firmware using cyfx3 sdk 1.3, that can be able to write debug logs into USB CDC in super speed mode. We face situation like video stream stop after some time of continues streaming. We have collected logs and that was not give much information intern of diagnosing the issue. I would like to know about, how can we enable more log capability for situation like this. Sample of logs as below when issue occurs.
[2023-09-19 08:56:12.770] TimeDiff = 651 ms FPS = 46
[2023-09-19 08:56:12.793] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8791 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.814] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8792 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.836] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8793 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.859] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8794 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.881] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8795 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.903] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8796 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.925] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8797 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.947] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8798 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.969] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8799 Frm_Sz = 2048000 B
[2023-09-19 08:56:12.991] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8800 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.013] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8801 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.035] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8802 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.057] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8803 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.079] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8804 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.102] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8805 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.123] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8806 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.146] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8807 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.168] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8808 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.190] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8809 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.212] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8810 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.234] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8811 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.256] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8812 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.278] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8813 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.300] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8814 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.322] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8815 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.344] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8816 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.367] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8817 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.388] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8818 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.411] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8819 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.433] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8820 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.434] TimeDiff = 651 ms FPS = 46
[2023-09-19 08:56:13.457] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8821 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.477] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8822 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.499] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8823 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.521] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8824 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.543] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8825 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.565] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8826 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.587] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8827 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.610] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8828 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.632] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8829 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.654] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8830 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.676] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8831 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.698] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8832 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.720] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8833 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.742] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8834 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.764] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8835 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.787] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8836 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.809] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8837 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.830] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8838 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.853] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8839 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.875] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8840 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.896] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8841 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.919] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8842 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.954] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8843 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.963] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8844 Frm_Sz = 2048000 B
[2023-09-19 08:56:13.985] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8845 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.008] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8846 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.029] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8847 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.051] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8848 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.074] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8849 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.095] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8850 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.095] TimeDiff = 652 ms FPS = 46
[2023-09-19 08:56:14.119] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8851 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.140] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8852 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.162] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8853 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.184] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8854 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.213] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8855 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.235] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8856 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.256] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8857 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.279] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8858 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.300] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8859 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.323] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8860 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.346] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8861 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.367] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8862 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.390] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8863 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.412] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8864 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.434] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8865 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.457] bRType = 0x2, bRequest = 0x1, wValue = 0x0, wIndex = 0x83, wLength= 0x0
[2023-09-19 08:56:14.459] Prod = 55 Cons = 55 Prtl_Sz = 23120 Frm_Cnt = 8866 Frm_Sz = 2048000 B
[2023-09-19 08:56:14.481] AplnStop:SMState = 0xA
[2023-09-19 08:56:14.516] bRType = 0x1, bRequest = 0x3, wValue = 0x0, wIndex = 0x100, wLength= 0x0
[2023-09-19 08:56:14.516] StpCB:In SET_FTR 0::1
[2023-09-19 08:58:31.860]
[2023-09-19 08:58:31.860] bRType = 0x1, bRequest = 0x3, wValue = 0x0, wIndex = 0x0, wLength= 0x0
[2023-09-19 08:58:31.860] StpCB:In SET_FTR 0::1
[2023-09-19 08:58:31.860] bRType = 0x1, bRequest = 0x3, wValue = 0x0, wIndex = 0x100, wLength= 0x0
[2023-09-19 08:58:31.860] StpCB:In SET_FTR 0::1
Thank
Dinusha
Show LessHi,
I am trying to connect the infineon gate driver for high voltage GaN MOSFET and I have designed the attached Altium circuit. Can you tell me what is incorrect here and what can be done.
Thanks is advance.
Neha Agarwal
Show LessI am considering providing backup power to the Vcc pin of the ILD8150XUMA1. Under normal circumstances, we plan to supply approximately 60V to the Vin pin. However, there are potential fault conditions where the voltage may drop to as low as 1V. In such situations, we want the internal logic of the chip to continue functioning normally. My question is: Will supplying a backup voltage of around 6.8V to the Vcc pin in the absence of Vin cause any issues or complications?
I understand VCC provides the output voltage from internal regulator but still can this be use to provide 6.8V externally.
Show Less
Hello,
I wanted to measure the CPU load using DMIPS. Could you please brief me with the procedures on how it can be done?
Looking forward to your response!
Thanks in advance! 🙂
Hey fellow Engineers,
I have the #EVAL-M5EVAL-M5-IMZ120R-SIC, which is a 3-phase inverter board, and I want to make it work with a 48V DC-link voltage. In the manual, it's mentioned that changing one of the resistors will allow the auxiliary supply to trigger at a lower voltage.
"For example changing the resistor value of R668 from 14 kΩ(default value) to 39 kΩ will alow AUX supply to trigger at lower DC voltage of around 200V instead of 400 V."
Is there a formula available to determine how to change that specific resistor? I've attempted to comprehend the #ICE5QSAGIC to understand how to make these modifications, but I'm struggling with it. Can anyone provide assistance?
Cheers, Steven
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023