Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

All Forums

Browse the Community

USB

Universal Serial Bus (USB) forums have discussions regarding Low-Full & High Speed Peripherals, Superspeed Peripherals, USB Hosts Hubs Transceivers, and USB EZ-PD Type C product solutions for PCs and consumer device topics.

80072558 12336

Memories

Memory Discussion Forums discussions regarding NOR Flash, SRAM, nvSRAM and F-RAM - performance and reliability with discrete memory densities ranging from 4K-bit to 2G-bit topics.

13235459 2947

Other Technologies

Discussion forum regarding Other Technologies including Power Management and Clocks topics.

1569993 834

Software

Software including ModusToolbox, PSoC Creator, WICED Studios and Wi-Fi Bluetooth for Linux .

118974256 15383

Battery Management ICs

Infineon's TLE9012DQU is a multi channel battery monitoring and balancing IC for various lithium-ion battery applications, with integral functions like voltage and temperature measurement, cell balancing, and isolated communication with the main battery controller, including self-diagnosis features. The TLE9015DQU iso UART Transceiver IC is used in battery systems for enabling the communication between the main microcontroller and multiple TLE9012DQU units in a daisy-chain configuration. This forum welcomes discussions, queries, and insights on battery management systems and devices.

25581 62
filter icon

Featured Discussions

sonju
AURIX™
Hi. I would like to use iLLD_TC375_ADS_FFT_Frequency_Analyzer_Microphone example project from TC375 in TC397. Because my purpose is to FFT process the... Show More
Marcelo_Macedo1
XMC™
Hi, Are you aware of any reference design or code example tailored for controlling Switched Reluctance Motors (SRM)? It could be using Dave or ModusTo... Show More
megatops
AURIX™
Hi, I've 2 TriBoards connected to my computer via the embedded miniWigglers, running different codes (client & server). But each time I use the Aurix ... Show More
TeHe_3863356
PSoC™ 4
Greetings.  I need to create a BSP in Modus Toolbox for the CY8C4248LQI-BL583T, a PSoC  4 device.  This is not an available option in the BSP Assistan... Show More
Kevingiordano14
AURIX™
hello everyone,I wanted to ask you for an explanation of how DMA works when setting up a transaction made by two transfers.In my case, I would like to... Show More
Kevingiordano14
AURIX™
Hi community, i have a Triboard TC3x9 which mount an AURIX TC39.  Yesterday I was using the board when all of a sudden I heard a sparking noise coming... Show More
Eason_Tsai
MOSFET (Si/SiC)
Dear Sir, I am going to design a 9kW DC-DC ESS solution. I found REF_DAB11KIZSICSYS11kW design and would like to purchase the EV kit , however, the ke... Show More
WEN-YUNG
MOSFET (Si/SiC)
Dear IFXer, May I know the turn off loss of high side MOSFET can be show as following? because I still not understanding the Eoss if that including Eo... Show More
MichelSole
AIROC™ Bluetooth
Hi, I've been trying to get the GATT responses working (Read Requests mostly), but I seem to be having some issues. Here is the behavior that I am get... Show More
iCatlett
Power Management ICs
Hello, I made a custom board with the WLC1115 wireless transmitter chip. I am not sure whats happening, but the VDDD pins on the chip are producing 1.... Show More