cancel
Showing results for 
Search instead for 
Did you mean: 

FM0+, FM3 & FM4 MCU

Anonymous
Not applicable

i'd just perform a "chip erase" on S6e1c by SW-DP(whithout rewrite CR zone in). and then, it dos not work anymore.

0 Likes
1 Solution
bharadhwajas_91
Employee

You may have to re-write the CR trim values if it is lost. Please refer to http://www.cypress.com/file/222996/download chapter 2 of the Peripheral manual.

   

Attaching a template project which as reference for FM3 which re-writes CR trim.Please note that this is a reference only and not in standard PDL format, you may have to use similar logic but modify for your device(pwd:cypress)

View solution in original post

0 Likes
2 Replies
bharadhwajas_91
Employee

You may have to re-write the CR trim values if it is lost. Please refer to http://www.cypress.com/file/222996/download chapter 2 of the Peripheral manual.

   

Attaching a template project which as reference for FM3 which re-writes CR trim.Please note that this is a reference only and not in standard PDL format, you may have to use similar logic but modify for your device(pwd:cypress)

View solution in original post

0 Likes
Anonymous
Not applicable

got,i would have a try later, Thank U!

0 Likes
Top labels