Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
As has been reported elsewhere, I am getting "The given PDL path "C:\Program Files (x86)\Cypress\PDL\3.1.7" is invalid. Unable to find required PDSC file." when I attempt to Generate Application. I am trying to run the "Hello World" application, i.e. just getting started with PSoC 6. The path should be valid since I found it via the "Browse" button.
Can someone advise me how to fix this?
Thank you.
Show Less
I can program the psoc5 using openocd now, with some caveats. However, if an NVL entry exists, it stops.
I have a project which somehow did something to the NVL.
I understand setting the Reset condition on the Pins can cause this. However, setting the pins to Don't Care doesn't fix this problem, so I suspect something else is causing the NVL to change.
Is there *any* gui / command line interface to find out what is causing the NVL to be set? (so it can be "fixed" in the project?)
This would not normally be a problem, but using openocd to program the psoc halts when the NVL entry is in the Creator generated hex file. I have multiple reasons for using openocd, some of which involve production machines. Others are very fast compile/debug cycle. (https://socmaker.com/?p=1004, and https://socmaker.com/?p=1027)
If I use objcopy, could I exclude that from the elf file for the new obj? (before making a hex file) If so, would it be by address? If so, which address? otherwise, how would I do that exclusion?
Is there a way to use openocd to program the NVL (perhaps kitprog in kitprog mode?) (Just checking)
Thanks!
Show Less
Info : Could not connect to device: MiniProg4/PSoC 61/62/63
Info : Open On-Chip Debugger 0.11.0+dev-4.4.0.2134 (2022-09-08-13:07)
Info : Licensed under GNU GPL v2
Info : For bug reports, read
Info : http://openocd.org/doc/doxygen/bugs.html
Info : DEPRECATED! use 'adapter speed' not 'adapter_khz'
Info : adapter speed: 1000 kHz
Info : adapter speed: 1500 kHz
Info : adapter speed: 1500 kHz
Info : >> do kp3 acquire
Info : Using CMSIS-DAPv2 interface with VID:PID=0x04b4:0xf151, serial=180F031D03201400
Info : CMSIS-DAP: SWD supported
Info : CMSIS-DAP: JTAG supported
Info : CMSIS-DAP: Atomic commands supported
Info : CMSIS-DAP: FW Version = 2.0.0
Info : CMSIS-DAP: Interface Initialised (SWD)
Info : SWCLK/TCK = 1 SWDIO/TMS = 1 TDI = 0 TDO = 0 nTRST = 0 nRESET = 1
Info : CMSIS-DAP: Interface ready
Info : KitProg3: FW version: 2.40.1241
Info : KitProg3: Pipelined transfers enabled
Info : KitProg3: Asynchronous USB transfers enabled
Info : VTarget = 3.319 V
Info : kitprog3: acquiring the device (mode: reset)...
Error: kitprog3: failed to acquire the device
Info : clock speed 1500 kHz
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
Error: Error connecting DP: cannot read IDR
Error: DAP 'test.cpu' initialization failed (check connection, power, transport, DAP is enabled etc.)
Info : Disconnected - MiniProg4 CMSIS-DAP BULK-180F031D03201400 FW Version 2.40.1241
I am getting above error while programming CY8C6245LQI-S3D42 using miniprog-4. There are 2 boards giving same problem. These boards were programmed earlier. Also the programmer setup is confirmed working using another board.
Can anyone help to resolve this issue?
Show LessI am attempting to follow the "Secure Boot" SDK user guide but continually run into the same problem. When attempting to setup the "CySecureTools" workspace i get the same error 'bash: cysecuretools: command not found' i get this even though i installed it and when i attempt to reinstall cysecuretools i got the message stating command already satisfied. This is all done on Windows
Show LessHi Team,
Couldn't find the CAN Mailbox definitions in SDL Libraries. Is there a way to configure the mailbox in TRAVEO 2 CYT2CL?
Thanks,
Pradeep
Hi
I am studying the Device Firmware Upgrade code
I can change the code and make it run the FW upgrade via UART by modifying the common.mk,
and I noted the differences when I used the original sample with the I2C interface, when the upgrade process is done, the PSoC6 cam restart/reboot. and running the cm4 code
but when I changed the interface to UART. it seems to upgrade successfully, but the EVK doesn't reboot
is there anything else I need to change besides the
TRANSPORT_OPT?=UART
please advise
Thanks
Show Less
Hi,
I want to know CYT2B75CAE this controller is supporting AUTOSAR, If yes where i will get those information,
when i browse i am not able to find the information
Show LessHello,
Recently if I open PSoC Designer normally (not as admin) I can open projects but the top file menu ribbon is not available and I can't do any build or debugging.
If I run Designer as admin then the project does not open and I get this error:
has anyone had this problem? Any help is appreciated.
Show Less
hi
i want to use the SCR in order to reduce the power consumption , and meet some block point. please check state flow bellowing :
if SW switch to SCR domain to execute, which position will sw execute next after wake up source login and exit from SCR domain ?
Step A (step A as the SW first code after reset )? or back to Step B?
Show Less
-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023