Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Microcontrollers Forum Discussions

Browse the Community

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.

22925561 4003

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy

61715797 9001

PSoC™ 5, 3 & 1

The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.

77123587 8716

CAPSENSE™ & MagSense

The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.

1014991 326

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs

17931158 4648

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.

2601411 806

MOTIX™ MCU

The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!

4243130 684
filter icon

Featured Discussions

DownyK
AURIX™
Hi members,   I have a question about How can I erase SMU ALM7[7]. This Alarm is related to the SPU Module, However, in this IC, There is no SPU Modul... Show More
Bhanuprasanth1
AURIX™
Im using tc377 for uart communication, I have to send data from tx  without interrupt by using Timer(Gpt12)when i using this Data is stored in Tx buff... Show More
khaledhassan
AURIX™
Hi, I can't add any printf or can't use UART from sample Ethernet application   if I add anything there it is crashing I need to process data after ... Show More
Shambhu
AURIX™
Hi, I am using Aurix TC375 Lite Kit development board and tried the freeRtos example code. But after compilation, once the code is put in the debugger... Show More
pblemel
PSoC™ 6
I am attempting to follow the "Secure Boot" SDK user guide but continually run into the same problem. When attempting to setup the "CySecureTools" wor... Show More
User22013
AURIX™
Hi, Where can I find the BSDL file for this Aurix IC TC367?
manishasagare4
AURIX™
I am using Application Kit TC3X7 V2.0 TFT board I have configured BMHD but  the board all the time boots from Internal flash ignoring BMHD settings If... Show More
MSS
PSoC™ 6
Hi, I am using CY8C6245LQI-S3D42 and I used the DFU examples to boot the system and created the application to run on AM4 core and everything is worki... Show More
PrasadA
XMC™
Hello,I am trying to flash littlefs filesystem on the qspi external serial flash memory in XMC7100 V1.1. As I see library mtb-littlefs is not included... Show More
lovre23
Legacy microcontrollers
Hello everyone! Is it possible to directly measure the current running through a DC motor using the BTN9970LV shield? I tried finding the answer in th... Show More
Category Information

Microcontrollers

Discussions regarding PSoC and MCU products.