Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Microcontrollers Forum Discussions

Browse the Community

PSoC™ 6

Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.

23051711 4015

PSoC™ 4

PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy

61994776 9005

PSoC™ 5, 3 & 1

The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.

77473950 8721

CAPSENSE™ & MagSense

The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.

1023748 327

AURIX™

In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs

18167302 4672

TRAVEO™ T2G

Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.

2623529 814

MOTIX™ MCU

The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!

4287644 691
filter icon

Featured Discussions

taegyunahn
TRAVEO™ T2G
Hi, I'm using CYT4BF. I confirmed that the Bandgap Reference circuits can be set to higher current mode or low power in the PWR_CTL2.BGREF_LPMODE regi... Show More
tsd
XMC™
请教,我目前正在使用的是,XMC4800_E196K2048的芯片,工程是ETHCAT_SSC_AUT_BASE_XMC48,我在这个工程上添加了,PMSM_FOC的模块,但U,V,W三相引脚,无法配置P0_0,P0_1,P0_2,P0_3,P0_4,P0_5,这六个引脚。但我明明没有使用这个六引脚... Show More
DeepSpace
PSoC™ 5, 3 & 1
I am using the  CY8CKIT-059 PSoC 5LP Prototyping Kit  for a project, and I'm very new to this. I have been a LabVIEW programmer for ten years, so I'm ... Show More
wqh98
AURIX™
请教大家一个问题 我现在做的boot程序在跳转app程序的时候,如果boot程序和app程序都没有使用中断的情况下可以正常跳转,但是boot程序或app程序有一方面使用中断的话就会进入到debug,boot程序或app程序单独运行时没有问题。下面按照串口中断举例。 调试状态下会卡在下图位置: 我... Show More
Nikhil_U
AURIX™
Hello,   We are developing the bootloader for the Infineon TC377 board.  For that, we need the preserved RAM (The memory that shouldn't be initialized... Show More
dharni
TRAVEO™ T2G
大家好,      最近想用keil调试cyt2bt73cae这个芯片的程序,使用mtb导出的工程只有单核应用,然后device这里显示 ,这种导出的工程直接是CM4的,编译过后能够达到使用CM0启动CM4的效果?如果不能,我应该怎么做?  当我配置了cm0plus以后,cy_m0p_image[]... Show More
钱女有
AURIX™
Hi infineon As the title said, I got a problem with "Vddk", I use the next formula to configure "Vddk", but some products(not all, same program) will ... Show More
Translation_Bot
CAPSENSE™ & MagSense
HI Purchasing S29GL01GT11FHIV10 product, I would like to confirm why the silkscreen is not reflected in the complete, in the specification did not see... Show More
Smitty99
MOTIX™ MCU
I am trying to use the BLCD Shield. I am unable to update setparameter(), which led me down the rabbit hole of downloading Kiel uvision5, buying a j-l... Show More
L1sTea
AURIX™
Hi, I have a AURIX MotorControl Application Kit with TC234LF, I want to switch from ADS to Visual Studio Code. I'm going to make it through the GCC co... Show More
Category Information

Microcontrollers

Discussions regarding PSoC and MCU products.