Microcontrollers Forum Discussions
Browse the Community
PSoC™ 6
Discussion forum regarding PSoC™ 6 - 32-bit Arm Microcontroller (MCU) Forum, discusses the 40-nm technology - best combination of ultra-low-power consumption, flexibility, security and high-performance topics.
PSoC™ 4
PSoC™ 4 - Arm®-based Forum, discusses the low-power Cortex®-M0 and Cortex®-M0+ cores, CapSense®, and Bluetooth® Low Energy
PSoC™ 5, 3 & 1
The PSoC™ 5LP, PSoC 2 and PSoC 1 Forum discusses - 24-bit Digital Filter Block (DFB), 24 UDBs, DMA controller and integrating AFE, digital logic with user interface ICs with an Arm Cortex-M3 CPU solutions.
CAPSENSE™ & MagSense
The Sensing Technology Forum discusses CAPSENSE™ - capacitive-sensing and MagSense inductive-sensing for consumer, industrial, automotive, and Internet of Things (IoT) applications.
XMC™
AURIX™
In this forum you can post your questions, comments and feedback about the 32-bit AURIX™ TriCore™ Microcontroller. The AURIX™ offers the highest scalability in performance, memory & peripherals across application. It is a safe and secure companion chip, meeting both the ISO functional safety standards and EVITA full security standards. Here you can also find the links to the latest board pages, SW and Tools GitHub, trainings, documents and FAQs
TRAVEO™ T2G
Discussion forum regarding 32-bit TRAVEO™ T2G Microcontroller - based on ARM® for automotive body electronics applications; cutting-edge performance, safety, and security features topics.
MOTIX™ MCU
The MOTIX™ MCU forum is designed for you to post your questions, comments and feedback about the famous Embedded Power ICs at anytime. Ask your technical questions or explore existing content!
Legacy microcontrollers
Featured Discussions
I'm encountering a problem with CAN transmission in TC233, and I could really use some assistance in troubleshooting it.
The scenario is as follows: I've utilized code from the iLLD example source for CAN initialization. Initially, I developed code for TC234, where P20_8 and P20_7 pins were configured as CAN TX and CAN RX pins respectively. This code works perfectly fine in TC234.
However, when I attempted to adapt the same code for TC233, making the necessary adjustments such as changing the pins to P14_0 and P14_1 and updating the Node1 settings, the code doesn't function as expected in either TC233 or TC234.
I have shared the code below.
/********************************************************************************************************************
* \file MULTICAN.c
* \copyright Copyright (C) Infineon Technologies AG 2019
*
* Use of this file is subject to the terms of use agreed between (i) you or the company in which ordinary course of
* business you are acting and (ii) Infineon Technologies AG or its licensees. If and as long as no such terms of use
* are agreed, use of this file is subject to following:
*
* Boost Software License - Version 1.0 - August 17th, 2003
*
* Permission is hereby granted, free of charge, to any person or organization obtaining a copy of the software and
* accompanying documentation covered by this license (the "Software") to use, reproduce, display, distribute, execute,
* and transmit the Software, and to prepare derivative works of the Software, and to permit third-parties to whom the
* Software is furnished to do so, all subject to the following:
*
* The copyright notices in the Software and this entire statement, including the above license grant, this restriction
* and the following disclaimer, must be included in all copies of the Software, in whole or in part, and all
* derivative works of the Software, unless such copies or derivative works are solely in the form of
* machine-executable object code generated by a source language processor.
*
* THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE
* WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE, TITLE AND NON-INFRINGEMENT. IN NO EVENT SHALL THE
* COPYRIGHT HOLDERS OR ANYONE DISTRIBUTING THE SOFTWARE BE LIABLE FOR ANY DAMAGES OR OTHER LIABILITY, WHETHER IN
* CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS
* IN THE SOFTWARE.
*********************************************************************************************************************/
/*********************************************************************************************************************/
/*-----------------------------------------------------Includes------------------------------------------------------*/
/*********************************************************************************************************************/
#include "MULTICAN.h"
#include "string.h"
/*********************************************************************************************************************/
/*-------------------------------------------------Global variables--------------------------------------------------*/
/*********************************************************************************************************************/
AppMulticanType g_multican; /* Global MULTICAN configuration and control structure */
AppLedType g_led; /* Global LED configuration and control structure */
uint32 Battery_Saving_Mode, Low_Power_Mode, Mode,Motor_ON_OFF, MCU_ON_OFF;
/*********************************************************************************************************************/
/*---------------------------------------------Function Implementations----------------------------------------------*/
/*********************************************************************************************************************/
/* Macro to define Interrupt Service Routine.
* This macro:
* - defines linker section as .intvec_tc<vector number>_<interrupt priority>.
* - defines compiler specific attribute for the interrupt functions.
* - defines the Interrupt service routine as ISR function.
*
* IFX_INTERRUPT(isr, vectabNum, priority)
* - isr: Name of the ISR function.
* - vectabNum: Vector table number.
* - priority: Interrupt priority. Refer Usage of Interrupt Macro for more details.
*/
IFX_INTERRUPT(canIsrTxHandler, 0, ISR_PRIORITY_CAN_TX);
//IFX_INTERRUPT(canIsrRxHandler, 0, ISR_PRIORITY_CAN_RX);
IFX_INTERRUPT(canIsrRxHandler, 0, ISR_PRIORITY_CAN_RX);
/* Interrupt Service Routine (ISR) called once the TX interrupt has been generated.
* Turns on the LED1 to indicate successful CAN message transmission.
*/
void canIsrTxHandler(void)
{
/* Just to indicate that the CAN message has been transmitted by turning on LED1 */
// IfxPort_setPinLow(g_led.led1.port, g_led.led1.pinIndex);
IfxPort_togglePin(g_led.led2.port, g_led.led2.pinIndex);
}
void canIsrRxHandler(void)
{
volatile IfxMultican_Status readStatus[10];
memset(readStatus, 0, 10*sizeof(readStatus[0]));
for(int i = 1; i <= 2; i++)
{
Ifx_CAN_MO *hwObj = IfxMultican_MsgObj_getPointer(g_multican.canDstMsgObj.node->mcan, i);
if(hwObj->STAT.B.NEWDAT != 0)
{
IfxPort_togglePin(g_led.led2.port, g_led.led2.pinIndex);
g_multican.canDstMsgObj.msgObjId = i;
readStatus[i-1] = IfxMultican_Can_MsgObj_readMessage(&g_multican.canDstMsgObj, &g_multican.rxMsg);
}
}
}
/* Interrupt Service Routine (ISR) called once the RX interrupt has been generated.
* Compares the content of the received CAN message with the content of the transmitted CAN message
* and in case of success, turns on the LED2 to indicate successful CAN message reception.
*/
/*Function to initialize MULTICAN module, nodes and message objects related for this application use case */
void initMultican(void)
{
IfxMultican_Can_initModuleConfig(&g_multican.canConfig, &MODULE_CAN);
g_multican.canConfig.nodePointer[TX_INTERRUPT_SRC_ID].priority = ISR_PRIORITY_CAN_TX;
g_multican.canConfig.nodePointer[RX_INTERRUPT_SRC_ID].priority = ISR_PRIORITY_CAN_RX;
IfxMultican_Can_initModule(&g_multican.can, &g_multican.canConfig);
IfxMultican_Can_Node_initConfig(&g_multican.canNodeConfig, &g_multican.can);
g_multican.canNodeConfig.txPin = &IfxMultican_TXD1_P14_0_OUT;
g_multican.canNodeConfig.rxPin = &IfxMultican_RXD1B_P14_1_IN;
g_multican.canNodeConfig.loopBackMode = FALSE;
g_multican.canNodeConfig.nodeId = IfxMultican_NodeId_1;
g_multican.canNodeConfig.rxPinMode = IfxPort_InputMode_pullUp;
g_multican.canNodeConfig.txPinMode = IfxPort_OutputMode_pushPull;
// g_multican.canNodeConfig.alertInterrupt.enabled = FALSE;
IfxMultican_Can_Node_init(&g_multican.canSrcNode, &g_multican.canNodeConfig);
//IfxMultican_Can_Node_init(&g_multican.canDstNode, &g_multican.canNodeConfig);
TX_CAN_ID_Init();
RX_CAN_ID_Init();
}
void TX_CAN_ID_Init(void){
IfxMultican_Can_MsgObj_initConfig(&g_multican.canMsgObjConfig, &g_multican.canSrcNode);
/*** The msgObjId for CAN TX must be different from all CAN RX msgObjId ***/
g_multican.canMsgObjConfig.msgObjId = SRC_MESSAGE_OBJECT_ID;
g_multican.canMsgObjConfig.messageId = CAN_MESSAGE_ID; // 0x777
g_multican.canMsgObjConfig.frame = IfxMultican_Frame_transmit;
g_multican.canMsgObjConfig.txInterrupt.enabled = TRUE;
g_multican.canMsgObjConfig.txInterrupt.srcId = TX_INTERRUPT_SRC_ID;
IfxMultican_Can_MsgObj_init(&g_multican.canSrcMsgObj, &g_multican.canMsgObjConfig);
}
void RX_CAN_ID_Init(void){
IfxMultican_Can_MsgObj_initConfig(&g_multican.canMsgObjConfig, &g_multican.canDstNode);
/*** Each Message Object ID is attached with unique CAN ID ***/
g_multican.canMsgObjConfig.msgObjId = DST_MESSAGE_OBJECT_ID;
g_multican.canMsgObjConfig.messageId = 0x333;
g_multican.canMsgObjConfig.frame = IfxMultican_Frame_receive;
g_multican.canMsgObjConfig.rxInterrupt.enabled = TRUE;
g_multican.canMsgObjConfig.rxInterrupt.srcId = RX_INTERRUPT_SRC_ID;
IfxMultican_Can_MsgObj_init(&g_multican.canDstMsgObj, &g_multican.canMsgObjConfig);
g_multican.canMsgObjConfig.msgObjId = DST_MESSAGE_OBJECT_ID+1;
g_multican.canMsgObjConfig.messageId = 0x444;
g_multican.canMsgObjConfig.frame = IfxMultican_Frame_receive;
g_multican.canMsgObjConfig.rxInterrupt.enabled = TRUE;
g_multican.canMsgObjConfig.rxInterrupt.srcId = RX_INTERRUPT_SRC_ID;
IfxMultican_Can_MsgObj_init(&g_multican.canDstMsgObj, &g_multican.canMsgObjConfig);
}
void transmitCanMessage(void){
const uint32 dataLow = 0x11111111;
const uint32 dataHigh = 0x22222222;
/* Invalidation of the RX message */
IfxMultican_Message_init(&g_multican.rxMsg,
INVALID_ID_VALUE,
INVALID_DATA_VALUE,
INVALID_DATA_VALUE,
g_multican.canMsgObjConfig.control.messageLen);
IfxMultican_Message_init(&g_multican.txMsg,
CAN_MESSAGE_ID,
dataLow,
dataHigh,
g_multican.canMsgObjConfig.control.messageLen);
IfxMultican_Can_MsgObj_sendMessage(&g_multican.canSrcMsgObj, &g_multican.txMsg);
}
void initLed(void){
/* ======================================================================
* Configuration of the pins connected to the LEDs:
* ======================================================================
* - define the GPIO port
* - define the GPIO pin that is the connected to the LED
* - define the general GPIO pin usage (no alternate function used)
* - define the pad driver strength
* ======================================================================
*/
g_led.led1.port = &MODULE_P13;
g_led.led1.pinIndex = 0;
g_led.led1.mode = IfxPort_OutputIdx_general;
g_led.led1.padDriver = IfxPort_PadDriver_cmosAutomotiveSpeed1;
g_led.led2.port = &MODULE_P13;
g_led.led2.pinIndex = 1;
g_led.led2.mode = IfxPort_OutputIdx_general;
g_led.led2.padDriver = IfxPort_PadDriver_cmosAutomotiveSpeed1;
/* Initialize the pins connected to LEDs to level "HIGH"; will keep the LEDs turned off as default state */
IfxPort_setPinHigh(g_led.led1.port, g_led.led1.pinIndex);
IfxPort_setPinHigh(g_led.led2.port, g_led.led2.pinIndex);
/* Set the pin input/output mode for both pins connected to the LEDs */
IfxPort_setPinModeOutput(g_led.led1.port, g_led.led1.pinIndex, IfxPort_OutputMode_pushPull, g_led.led1.mode);
IfxPort_setPinModeOutput(g_led.led2.port, g_led.led2.pinIndex, IfxPort_OutputMode_pushPull, g_led.led2.mode);
/* Set the pad driver mode for both pins connected to the LEDs */
IfxPort_setPinPadDriver(g_led.led1.port, g_led.led1.pinIndex, g_led.led1.padDriver);
IfxPort_setPinPadDriver(g_led.led2.port, g_led.led2.pinIndex, g_led.led2.padDriver);
}
Show Less
Is there a Dave App function or XMC function available that enables the connection of two pins to each other?
使用cy8c6347,请问如何很精确的发出固定数目的脉冲?使用定时器好一点还是利用脉冲产生的中断来计数更精确?
in TC38x,Can the local memory unit(LMU) and thre Distributed LMU (DLMU) as a whole LMU to be used in OVC function SAL-TC387QP-160F300S AD
Show Less你好
目前使用"UART_VCOM_1_KIT_TC397_TFT"範例在Triboard TC397上進行測試。
開啟兩組ASCLIN 模組0跟模組4並且在中斷設置中有更改相對應的向量表數值,進行以下交互測試:
1. CPU0_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(0)"跟進行輸出"Hello World!" ==> 可以正常顯示
2. CPU1_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(1)"跟進行輸出"Hello World!" ==> 無法顯示
3. CPU2_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(2)"跟進行輸出"Hello World!" ==> 可以正常顯示
4. CPU3_Main.c內執行兩組ASCLIN初始化、只有調整"中斷向量表數值(3)"跟進行輸出"Hello World!" ==> 可以正常顯示
想請問為何在CPU1_Main.c會有此問題?
#AURIX
#Tricore
Show Less
when try to debug the example project through miniwiggler, it can not work as below:
but memtool can connect the chip :
MCD basic client can also connect the chip and get the information:
the ADS version is 1.9.20 ,DAS version is 8.0, miniwiggler is V3.1, hardware board is designed by other people and can be connected through UDE/pls
Show Less
Dear Forum:
I know that
The Hex file generated by the Modus Tool box IDE follows the Intel Hex File format which is supported by the Cypress Programmer.
from the following title.
https://community.infineon.com/t5/PSoC-6/PSoC-programmer-parsing-failure/td-p/716946
I want to confirm that
Which IDE can generate hex file used by PSoC programmer?
Thank you.
Show LessDear team need to understand why the upper limit for overtemperature is locked?
Also please confirm if there is any sample code for handling overtemperature
Show Less
Dear Team,
I am using the sequencer for analog input reading, just want to know what is difference between interrupt method and sequencer method for ADC1 reading?
Show Less-
TraveoII
UART buadrate Setting
by chandan1995 Jun 19, 2023