- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi
So i found a bug in the PDL Library v2.1.0
The function Mfs.I2c_ConfigAck() doesn't work like it is in the library.
I had to change it like this to get it working:
/**
******************************************************************************
** \brief Configure ACK signal sent to master
**
** \param [in] pstcI2c Pointer to I2C instance
** \param [in] enAck ACK to be sent
** \arg I2cAck ACK will be sent as response signal
** \arg I2cNAck NACK will be sent as response signal
**
** \retval Ok ACK signal has been successfully configured
** \retval ErrorInvalidParameter If one of following conditions are met:
** - pstcI2c == NULL
**
** This function is only meaningful when I2C is in slave mode
**
******************************************************************************/
en_result_t Mfs_I2c_ConfigAck(volatile stc_mfsn_i2c_t* pstcI2c, en_i2c_ack_t enAck)
{
if(pstcI2c == NULL)
return ErrorInvalidParameter;
if(I2cAck == enAck){
*((volatile uint8_t *)(0x42000000UL + ((uint32_t)(pstcI2c - 0x40000000UL) * 32) + (13 * 4))) = 1; //ACKE set
}else{
*((volatile uint8_t *)(0x42000000UL + ((uint32_t)(pstcI2c - 0x40000000UL) * 32) + (13 * 4))) = 0; //ACKE clear
}
return Ok;
}
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
Which is the IDE and version used? Please confirm whether this issue occurs in IAR IDE.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
IDE: Keil uVision V5.17.0.0
ARM Compiler: V5.06 update 1 (build 61) (comes built into uVision)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content