Announcements

Curious on how you can apply Diodes to Smart Home Appliances? Register for the ASEAN Smart Home Appliance Webinar here to find out how.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Diodes & Thyristors (Si/SiC) Forum Discussions

MS_19060803
Level 5
50 questions asked 50 replies posted 100 sign-ins
Level 5

Hi all,

They would like to use the TZ400N26KOF at 5400Vac(RMS, f = 50 Hz, t = 1 min).
However, the insulation voltage of TZ400N26KOF is 3000Vac(RMS, f = 50 Hz, t = 1 min).

Then, I have a question.

If you know which insulation sheet to use at as much as 5400Vac, please let me know.
Also is there another way except for insulation sheet?

Best regards,

MS

0 Likes
1 Solution
AZIZ_HASSAN
Moderator
Moderator 100 sign-ins 50 solutions authored 10 likes received
Moderator

Hi,

Thank you for posting on Infineon community.

First of all this insulation voltage is applied between the all shorted terminals and the body( generally back plate) of the device. So, the insulation voltage is the property of the material used in the device. I think its really difficult to insert a sheet to increase the insulation voltage because where to insert is the main question.

However, still if you are able to insert the insulation sheet, I will suggest you few material for this.

1) PET( Polyethylene terephthalate) sheet - sheet thickness of 0.25mm  will be sufficient as per your voltage  requirement.

2) Mayler sheet- 0.25 mm thickness or greater.

3) GPO3 material- not sure about the thickness as per the voltage level.

 

BR,

AZIZ HASSAN

View solution in original post

0 Likes
1 Reply
AZIZ_HASSAN
Moderator
Moderator 100 sign-ins 50 solutions authored 10 likes received
Moderator

Hi,

Thank you for posting on Infineon community.

First of all this insulation voltage is applied between the all shorted terminals and the body( generally back plate) of the device. So, the insulation voltage is the property of the material used in the device. I think its really difficult to insert a sheet to increase the insulation voltage because where to insert is the main question.

However, still if you are able to insert the insulation sheet, I will suggest you few material for this.

1) PET( Polyethylene terephthalate) sheet - sheet thickness of 0.25mm  will be sufficient as per your voltage  requirement.

2) Mayler sheet- 0.25 mm thickness or greater.

3) GPO3 material- not sure about the thickness as per the voltage level.

 

BR,

AZIZ HASSAN

0 Likes