Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

Community Translations

JuIn_1625121
Level 5
100 sign-ins First solution authored 100 replies posted
Level 5

Hi

I want to translate KBA88957.

Please confirm to my work.

Best Regards,

Inoue

0 Likes
2 Replies
JennaJo
Moderator
Moderator 1000 replies posted 750 replies posted 500 replies posted
Moderator

Hi, Inoue-san

Confirm to work this KBA.

Thanks

Jenna

Jenna Jo
0 Likes
JuIn_1625121
Level 5
100 sign-ins First solution authored 100 replies posted
Level 5

Original:Crystal Requirements for EZ-USB® HX2LP™ and HX2VL™ – KBA88957

======================================================================

タイトル:EZ-USB® HX2LP™およびHX2VL™向け水晶振動子の要求仕様 - KBA88957

質問:EZ-USB® HX2LP™(CY7C65620/CY7C65632/CY7C65640)とHX2VL™(CY7C65632/CY7C65634/CY7C65642)に使う水晶振動子の要求仕様は何ですか?

回答:

CY7C65620/CY7C65630/CY7C65640Bに使う水晶振動子の要求仕様は以下の通りです。

周波数: 24 MHz

動作モード: 基本波モード、並列共振

周波数安定度: ±500 ppm

等価直列抵抗: ≤60 ohms

負荷容量: 12 pF

励振レベル: 500 μW

外部負荷容量は12pFとしてください。アイパターンの信号品質を向上させるために±100ppmの水晶を使用することが推奨されています。

CY7C65632/CY7C65634/CY7C65642に使う水晶振動子の要求仕様は以下の通りです。

周波数: 12 MHz

動作モード: 基本波モード、並列共振

周波数安定度: ±500 ppm

負荷容量: 20 pF

励振レベル: 600 μW

外部負荷容量は20pFとしてください。アイパターンの信号品質を向上させるために±100ppmの水晶を使用することが推奨されています。

0 Likes
Top labels