Community Translation - CYW20706 Schematic Design Considerations - KBA222368

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
KoSa_1909416
Level 5
Level 5
Distributor - Marubun (Japan)
250 sign-ins 25 replies posted First solution authored

I tried to translate this KBA222368 into Japanese.

https://community.cypress.com/docs/DOC-14315

----------------------------------------------------------------
タイトル:CYW20706回路設計に関する考慮事項-KBA222368

質問:
CYW20706の回路設計で考慮することは何ですか?

回答:

1.SDKのdoc ディレクトリにあるCYW92070aWCDEVAL-Hardware-User-Guide.pdfより、CYW920706_evalボードの回路図を参照してください。
2.電源部:評価ボードからコピーします。
3.外付け水晶発振器:CYW20706は、適切な外部ピン設定を選択することにより、20、24、40 MHzの水晶をサポートします。

ピン設定

発振周波数

BT_XTAL_STRAP_1BT_XTAL_STRAP_0
Low 固定Low 固定40 MHz
Low 固定High 固定24 MHz
High 固定Low 固定20 MHz

4.パッチとアプリケーションコードをダウンロードするには、外部にEEPROMまたはフラッシュが必要です。SflashまたはEEPROMをSPI2に接続します。

5.HCI UARTは、ダウンロード/ RAMブート/HCIコマンドの送信又はUARTアプリケーション機能に使用できます。
  PUARTはアプリケーション機能に使用されます。

6.F8-BT_DEV_WAKEは、ホストにリクエストがあることをCYW20706に通知するピンです。

7.F7-BT_HOST_WAKEは、CYW20706にリクエストがあることをホストに通知するピンです。

8.RFデザイン:バンドパスフィルターはLFB212G45CG2D013が推奨されます。
                         アンテナ調整にはパイ型ネットワークが推奨されます。

9.ピンの割り当てについては、データシートを参照してください。

----------------------------------------------------------------

Best Regards,

Sakagami

0 Likes
1 Reply
JennaJo
Moderator
Moderator
Moderator
1000 replies posted 750 replies posted 500 replies posted

Hello, Sakagami-san

We receive your translation, it will be internally reviewed and be published to KBA to Community.

After upload, You will receive the points as the word of KBA.

Please note that due to the current volume of works, Please bear with me for the delayed the response.

It can be delayed, but it will be surely processed.

Thanks for your contribution to CDC!

Will keep you update the status.

Thanks,

Jenna Jo

Jenna Jo