Sep 21, 2021
11:56 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Sep 21, 2021
11:56 PM
Hello,
I have bought 3 DAPMINIWIGGLERUSBTOBO1 and I've connected them via USB to an USB-HUB.
Doing so, I've realized that via InfineonMemtool 4.5 I'm able to connect only to one MiniWiggler.... is there a way to configure the tool in order to recognize the 3 different wigglers and to switch to the one I want to select?
Attached the configuration I have on my laptop.
Thanks for support.
I have bought 3 DAPMINIWIGGLERUSBTOBO1 and I've connected them via USB to an USB-HUB.
Doing so, I've realized that via InfineonMemtool 4.5 I'm able to connect only to one MiniWiggler.... is there a way to configure the tool in order to recognize the 3 different wigglers and to switch to the one I want to select?
Attached the configuration I have on my laptop.
Thanks for support.
Solved! Go to Solution.
- Tags:
- IFX
1 Solution
Feb 07, 2022
09:44 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 07, 2022
09:44 PM
Hi,
The tool has an option Use IO Pod .This selection is available when using communication devices where multiple JTAG interfaces are available (e.g. UAD3). Select the target port you want. If (default) is selected, then the first available port is used.
Best Regards,
Vasanth
1 Reply
Feb 07, 2022
09:44 PM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Feb 07, 2022
09:44 PM
Hi,
The tool has an option Use IO Pod .This selection is available when using communication devices where multiple JTAG interfaces are available (e.g. UAD3). Select the target port you want. If (default) is selected, then the first available port is used.
Best Regards,
Vasanth