cancel
Showing results for 
Search instead for 
Did you mean: 

Clocks

jaic_4673826
New Contributor

Hi All,

Im ICT test engineer, is there any programming tools that able to program CY25100 where the device is already attached on board?

as i found out "CY3675 ClockMaker Clock Programming Kit" needs to remove the device in order to do the programming.

preferable the programming tools to have Batch file for execution.

thank  you so much!

Regards,

Jan

0 Likes
1 Solution
PradiptaB_11
Moderator
Moderator

Hi Jan,

The CY25100 device can be programmed by using the CY3675 clock maker kit along with the CY25100 adapter card. The device needs to be place inside the adapter card, programmed with the JEDEC file and then use in the application.

OR

If the requirements are high the parts can be factory programmed by Cypress.

Thanks,

Pradipta.

View solution in original post

0 Likes
1 Reply
PradiptaB_11
Moderator
Moderator

Hi Jan,

The CY25100 device can be programmed by using the CY3675 clock maker kit along with the CY25100 adapter card. The device needs to be place inside the adapter card, programmed with the JEDEC file and then use in the application.

OR

If the requirements are high the parts can be factory programmed by Cypress.

Thanks,

Pradipta.

View solution in original post

0 Likes