cancel
Showing results for 
Search instead for 
Did you mean: 

CapSense & Magsense

JiZh_4762651
New Contributor

1. CY8CMBR3102   I2C 配置为100KHz,从模式;ESD测试之前正常;

2. 按键是金属弹簧按键,高度10mm,触摸面10mm, 同时有一个3mm透明PVC面板;

3. ESD测试,接触 6KV 对金属机箱进行测试(注:空气放电测试通过),CY8CMBR3102 I2C为纯粹的高电平,无数据信号(但CS0 触摸按键接口扫描信号正常),重启电源恢复正常;

0 Likes
5 Replies
LinglingG_46
Moderator
Moderator

1:金属外壳和芯片地之间是怎么连接的?

2:在I2C总线上面做一些处理:

  Pull-up resistors (R1, R2), typical range1: 4.7 k - 10 k

  Series resistors (R3, R4), typical range1: 100  - 330 

  Filter capacitors (C1, C2), typical value1: 10 nF

pastedImage_0.png

0 Likes
JiZh_4762651
New Contributor

1:金属外壳和芯片地之间是怎么连接的?

金属外壳(大地)与芯片地(信号地)通过102K电容进行隔离;

0 Likes
LinglingG_46
Moderator
Moderator

可以尝试我上面对I2C的操作,看是否可以解决问题?

0 Likes
JiZh_4762651
New Contributor

已尝试,无效!

0 Likes
Vison_Zhang
Moderator
Moderator

金属外壳与芯片地之间的电容还是去掉比较好。

建议你看一下这篇文章 不同外壳材质的防静电设计技巧,对你现在遇到的问题应该有帮助。

0 Likes