cancel
Showing results for 
Search instead for 
Did you mean: 

Bluetooth SDK

LUAB_4724786
Contributor

Hi there,

Since recently we purchase CYBT-213043-MESH EZ-BT™ Module Mesh Evaluation Kit which utilise CYBT-213043-02 EZ-BT MODULE, I would like to ask that do I need to have additional component in order to use it (eg. additional xtal, resistor, etc) ? or we could just utilise the pinout based on its functional according to its datasheet ?

And ... if we order it, the module that we are going to receive will be like in the image below right ?

CYBT-213043-MESH_4_Module.png

one more thing, in order to program it, could we just use the UART and use existing Modus Toolbox just like in the mesh evaluation kit ? or ... do I need other tools like usb to serial or other ?

Thanks for the helps.

Best Regards,

LUTHFI AD

0 Likes
1 Solution
DheerajPK_41
Moderator
Moderator

Hi,

CYBT-213043-02 is fully integrated and certified ready to use solution that provides all necessary components required to operate Bluetooth communication standards.

Yes, you will be getting a module as shown in the image.

Yes, you need use USB to Serial converter. Please check the module evaluation kit schematics given above.

The CYBT-213043-02 includes connections for an external 32-kHz oscillator to provide accurate timing during low power operations.

Note that, a 24.000 MHz, 12PF (Y1) crystal is a critical component used in the CYBT-213043-02 module. (Check page 12, 13).

Thanks,

-Dheeraj

View solution in original post

0 Likes
3 Replies
DheerajPK_41
Moderator
Moderator

Hi,

CYBT-213043-02 is fully integrated and certified ready to use solution that provides all necessary components required to operate Bluetooth communication standards.

Yes, you will be getting a module as shown in the image.

Yes, you need use USB to Serial converter. Please check the module evaluation kit schematics given above.

The CYBT-213043-02 includes connections for an external 32-kHz oscillator to provide accurate timing during low power operations.

Note that, a 24.000 MHz, 12PF (Y1) crystal is a critical component used in the CYBT-213043-02 module. (Check page 12, 13).

Thanks,

-Dheeraj

View solution in original post

0 Likes
LUAB_4724786
Contributor

Dear Dheeraj,

Thank you for the answer, I am following your recommendation of the document and found the external components required  just like in the picture below.

Screen Shot 2020-07-17 at 17.58.01-side.png

But what I dont understand next is "critical component", does it mean that I have to add it as external component later on ? or ... its already in the module ? because I cant find the pin to connect to that 24.000 MHz xtal.

Screen Shot 2020-07-17 at 19.03.15-side.png

Best Regards,

LUTHFI AD

0 Likes
DheerajPK_41
Moderator
Moderator

Hi,

"Critical Components" are the main components used in the CYBT-213043-02 module. These components are already present inside the module.

Thanks,

-Dheeraj