AURIX™ Forum Discussions
Hi Infineon team,
I have a TC387 kit, I need communicate to other device via SPI, and the device need 8 clk cycle, so I set the data width as 7:
Then config the set:
My Tx data is:
But I get incorrect data in Logic Analyzer:
When I set the SPI_DATA_WIDTH = 8 with 9 pulse, the data is right. Have I miss some setup?
Thank you,
Best wishes,
Sc
Show LessHello everyone,
I would like to access the datasheet for HSM TC275. Could you help me ?
I search and I found this one (https://www.infineon.com/dgdl/Infineon-TC27xDC_DS_v10-DS-v01_00-EN.pdf?fileId=5546d46259d9a4bf015a846b292f74ce ) but it is not the one that I am looking for.
Could you help me ?
Best regards,
Show Less
I am using Triboard eval board with device TC35x but it is not visible in Aurix development studio v1.9.0. Please help?
Hello, I am a CSE undergrad, and I have bought the shield buddy tc375 aurix micro controller board. I've been looking for a complete guide on programming and firmware development on the tc375 but there are very few resources available. And all the datasheets seem very overwhelming. And that's why it's getting quite hard to start working on the board as a beginner.... Please provide if you have a complete guide for embedded programing and firmware development on aurix. Also I've come to know about modusToolBox and aurix development studio. Please clarify which one should I use for shield buddy tc375 programming. This is a question as a beginner. Please ignore any silly mistakes.
Hi!
I have a question regarding Data Flash erase disturb limit. In KBA234714 (AURIX™ MCU: Data Flash erase disturb limit paramet... - Infineon Developer Community) it is mentioned that more than 50 erase cycles on a dflash sector may cause disturbances in neighbouring cells. However, it is not explained what is meant by neighbouring cells.
For example if 100 erase cycles are performed on dflash sector 3, does this mean disturbances may appear in dflash sector 2 and sector 4, or can disturbances appear in any dflash sector?
Show LessWe would like to use traction motor as well as compressor motor with single controller
Can some one suggest which controller can be best used?
Show Less
I want to set SCR DAP0/1 on TC39XB.
Setting SCR_P00.6 works fine.
However, when setting SCR_P00.7, an error occurs (X appears on the setting screen).
I don't understand why the error occurs.
Please tell me how to resolve.
@@@
Show Less