Trying to port the WHD driver, (WITHOUT WICED IDE), there are some include files like "wiced_resource.h" under resources-> clm -> component4343w. Is the "wiced_resource.h" a WICED filesystem? Is it specifically for WICED environment only?If yes, then I believe that still I can use the same APIs but with other (internal/extrenal) file system, right? If the resource module comes into the picture while FW Download Module?
The doc mentions that -
* The Resource could be one of the three locations
* - Wiced Filesystem (File System)
* - Internal Memory (Embedded Flash memory)
* - External Storage ( External Flash connected via SPI interface)
so, if I am not using Wiced Filesystem (as I am not using Wiced IDE), I shall use either of the other two options (internal/external). And the offered API such as resource_read, resource_get_readonly_buffer, etc. can be used. Is this correct? Please correct me if wrong & provide some more info. Thanks !!
Solved! Go to Solution.
Hi @aniruddhann ,
Yes, if you are not using Wiced IDE , you can use either of the other two options (internal/external) locations.
And you can use the Resource Management API's present.
Thanks,
Rakesh B G
Hi @aniruddhann ,
Yes, if you are not using Wiced IDE , you can use either of the other two options (internal/external) locations.
And you can use the Resource Management API's present.
Thanks,
Rakesh B G