Hello
I am trying to import this the Bluetooth HID Keyboard application into ModusToolbox, from this link https://github.com/Infineon/mtb-examples-CYW920819EVB-02-btsdk-hid/tree/master/hid/dual_mode_keyboar... but I am getting an error.
In ModusToolbox > File > New > ModusToolbox Application > Select BSP as "CYW920819EVB-02" > At the "Select Application" page, click "Import" > Navigate to "mtb-examples-CYW920819EVB-02-btsdk-hid/hid/dual_mode_keyboard" directory which I had already downloaded into my computer and click "Choose" > Check the "dual_mode_keyboard" checkbox and click "Create" > Error is as shown below:
Application "/home/user/Downloads/mtb-examples-CYW920819EVB-02-btsdk-hid-master/hid/dual_mode_keyboard" is not compatible with the BSP "CYW920819EVB-02".
Failed to collect application data for the "dual_mode_keyboard" application.
The application(s) creation failed. No valid application(s) selected.
Seems like the board model is already in the makefile :
# default target
TARGET=CYW920819EVB-02
#TARGET=CYW920819EVB-02
#TARGET=CYW920820EVB-02
#TARGET=CYW920735Q60EVB-01
SUPPORTED_TARGETS = \
CYW920819REF-KB-01 \
CYW920819EVB-02 \
CYW920820EVB-02 \
CYW920735Q60EVB-01 \
Are there any solutions to resolve this error?
Solved! Go to Solution.
Hello @HotPotTofu ,
Please note the HID Keyboard application is supported only under CYW920735Q60EVB-01 and CYW920819REF-KB-01 . So when you try it with different BSPs , you have to check the pins and configurations in the sample project.
Make sure you are using latest MTB IDE and then please try the below steps flow :
1. Import the example project to work space under the BSP CYW920819REF-KB-01
2. After successfully importing the project, now change the target name and supported targets for the CYW920819EVB-02 .
# default target
TARGET=CYW920819EVB-02
SUPPORTED_TARGETS = \
CYW920735Q60EVB-01 \
CYW920819REF-KB-01 \
CYW920819EVB-02
3. Now change the active BSP files using library manager. Click on Library manager in workspace explorer -> select the bsp file as CYW920819EVB-02 -> update (refer the screenshots attached)
4. Now please try clean and build. It worked at my side. Please let us know if you face any difficulties.
Regards,
Anjana