cancel
Showing results for 
Search instead for 
Did you mean: 

AIROC™ Bluetooth

jward2
New Contributor II

Hello,

I am very new to the world of PSoCs and my first exposure is a project I am working on using a CY8CPROTO-063-BLE. I am currently using "retarget I/O" and a UART block to establish communications over USB. However, I am trying to implement USB communications through a USBFS block to take advantage of full USB capabilities. I downloaded the code example CE223368 link here and changed the target device to CY8CPROTO-063-BLE. Upon doing this, I received a clock error stating that "The selected device does not support USB" (see image below) and I am unable to get the required clock frequency and accuracy to 48 MHz, +-0.25%.

Does the CY8CPROTO-063-BLE support using a USBFS block?

jward2_0-1634133573913.png

 

0 Likes
1 Solution
AnjanaM_61
Moderator
Moderator

Hello @jward2 ,

The module which you have selected does not support USB functionality. 

Refer https://community.cypress.com/t5/PSoC-6-MCU/CYBLE-416045-02-USB/m-p/170799

Regards,

Anjana

View solution in original post

0 Likes
4 Replies
AnjanaM_61
Moderator
Moderator

Hello @jward2 ,

The module which you have selected does not support USB functionality. 

Refer https://community.cypress.com/t5/PSoC-6-MCU/CYBLE-416045-02-USB/m-p/170799

Regards,

Anjana

0 Likes
jward2
New Contributor II

Hi @AnjanaM_61 ,

That is unfortunate, but thank you for confirming my suspicions. I suppose using a UART block will have to do.

Thank you

James

0 Likes
MotooTanaka
Esteemed Contributor

Hi,

If all you want is to use the USB connector to communicate with PC,

you can use P5[1], P5[0] with UART component.

Something like the attached project.

If I'm missing the point, I'm sorry.

moto

0 Likes
jward2
New Contributor II

Thanks for your reply @MotooTanaka .

I am currently using a UART component, I was trying to see if this particular PSoC supported full USB functionality (USB 2.0 compatible). Anjana above answered that already and it does not support full USB functionality, so a UART block will have to suffice.

Thanks again 😊