Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 109664 Discussions

  • 114827 Members

  • 68819 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
Guna
TRAVEO™ T2G

For 1 to 1 trigger ,SAR ch is decided based on logical channel or  ADC channel number?

ZJ01
AURIX™
Hi, I was recently working with TC387. I need to save some variables during standby mode, and after waking up, their value should not be initialized. ... Show More
Manimuthu
Power Management ICs
Hi team,I am writing to inquire about the LLC controller for specific requirements of our system.We are currently using UCC25660 in a half-bridge LLC ... Show More
yangkang
AURIX™
Change the value of HWCFG[7:0] via PIN,Whether FTM needs to be modified? the FTM value is also derived from the pin? Show More
Wendy2
MOTIX™ MCU

大家好 请问有没有关于TLE9879的CSA例程,BLDC电机控制里想加一个电流检测,官方例程里没有关于CSA的例子,希望有使用过这个功能的分享一下经验。 谢谢!

azeemhad
AURIX™
If i purchase KIT_A2G_TC399_5V_TRB_S HW then 1) Will it have the Chip SAK-TC399XE-256F300S BD, mounted on it? OR2) What chip (give me full name) , wil... Show More
Wendy2
MOTIX™ MCU
大家好 : 关于ADC和DMA 有几个疑问,想得到帮助。 1.官方例程TLE9879_DMA_ADC1中,adc_ch_result[DMA_CH0_NoOfTrans]数组设置为8,但是IFXCONFIG里面,图1所示序列模式勾选了14个(7个通道+7个通道4重复采集),那么这个地方,DMA在传数... Show More
Microcontroller
AURIX™
Hello all,I am able to see UCB_PLFASH register on my TC38x.But UCB_DFLASH  I am unable to see. Initially I was able to see and modify also with Trace3... Show More
yolominwoo
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
When i porting stm32h745 + Laird(lwb+), but stoped install firmware. I think bluetooth sensor can't init hello_sensor_application_init();    But nucl... Show More
Translation_Bot
USB hosts hubs transceivers
I would like to ask what would cause this error?   What I have in my code is to create an array of outputs on the INT side of EP0 in the UART callbac... Show More