Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

iMOTION™ controller, driver & IPM

Recent discussions

Sort by:
Airtech
iMOTION™ controller, driver & IPM
Hello, trying to drive an inverter refrigeration compressor, runs perfectly at low speeds (1200 to 2000rpm) but got gatekill motor fault when speed is... Show More
SBitney
iMOTION™ controller, driver & IPM
Hi,I'm having issues reaching higher currents when loading down a motor driven by a IMC101. I've got a maximum current limit of 3.5A set, and it will ... Show More
n6xb
iMOTION™ controller, driver & IPM
Greetings!  I have a few questions from a newbie. I am using the EVAL-M7-D111T and LVMOS driver board and have MCE Wizard parameters set for my 24V FA... Show More
sohail
iMOTION™ controller, driver & IPM
Hi,           i just got motoin2go board, install MCEDesigner but when i open file IMC101T_V1.02.20_iMOTION2go.irc it give error product mismatch.  i ... Show More
cw2611
iMOTION™ controller, driver & IPM

Hey!

I want to communicate with a gate driver from IMC302AF064XUMA1. How can I enable SPI communication using the MCE wizard?

cw2611
iMOTION™ controller, driver & IPM
Hey! I want to test IMC302AF064XUMA1 as a standalone without interfacing a gate driver to it. I want the microcontroller to generate PWM pulses which ... Show More
sohail
iMOTION™ controller, driver & IPM
Hi,          I am using EVAL-M3-302F board , In Kiel uvision  ide cant configure SW device Id code & Device name. I try MCE designer but  mce device c... Show More
cw2611
iMOTION™ controller, driver & IPM
Hello  I am trying to configure the BLDC motor using the MCE wizard, can the motor directly be operated using the MCE wizard? or do we need the SPI or... Show More
User20393
iMOTION™ controller, driver & IPM
Hi I can't find the Link Break Protection in Wizard 2.3.0.1. No idea where it is  pls guide me   Thanks Show More
sohail
iMOTION™ controller, driver & IPM
Hi,       I got new board EVAL-M3-302 trying to connect  but got error in Keil uvision5 ide & also in mce Designer. I think there is some problem in d... Show More
Forum Information

iMOTION™ controller, driver & IPM

iMOTION™ ICs integrate all the control and analog interface functions required for sensor less field oriented control (FOC) of PM motors using DC link or leg shunt current measurements. In this forum, you can post your questions about the iMOTION™ family and find resources for your next project.