Hi,
I am using IMC301-T064 device, I want to use UART1(user mode uart) as a brige between STM32F103 and IMC301. First of all, I set InterfaceConf0=23(UART1 in user mode) and InterfaceConf1=0(DISABLE JCOM), then programming codes into STM32F103, ENABLE UART(STM32F103, I/0 PA8 and P19), send instructions {0xFF,0x06,0x01,0x78,0x01,0x00,0xFF,0x80} to start the motor, but it failed. I use oscilloscope to see the signal of IMC301's Rx and Tx, the Rx can receive signal from STM32F103 normally, but there is no back signal on Tx. So what's my problem? Why there is no back signal?!
Solved! Go to Solution.
Hi @zlz,
Please ensure the user UART baud rate matches with STM32 ( by default User UART is configured to 57600 Baud rate)
Please find the below example command:
int Start_Command[8] = { 0x01, 0x03, 0x00, 0x00, 0x01, 0x01, 0xFE, 0xFB};
Start_Command :
0x01- Node address
0x03- Speed command
0x0000- Default value
0x0101 - Target speed 257 RPM
0xFBFE - Checksum ( -1 * ( 0x0301 + 0x0000 + ox 0101))
To get the reply from the Slave( iMotion) the baud rate must be configured correctly and the Motor command must be in a correct format.
Refer to section 2.3 ( User UART) for commands-https://www.infineon.com/dgdl/Infineon-MCESW-RM-UserManual-v01_03-EN.pdf?fileId=5546d462719b59230171...
Please let us know if you are able to start the motor by using the above command format.
Thanks,
Krupashankar
Hi @zlz,
According to my understanding, you have already programmed the IMC301 device with the necessary configurations, confirmed the working of the motor, and now want to control the motor using an external microcontroller. Please correct me if I am wrong.
We will check internally if we have an example script that you could use as a reference. Meanwhile, could you please share a snapshot of the Basic System Configuration Options or share the .mc2 file?
Hi @zlz,
Please ensure the user UART baud rate matches with STM32 ( by default User UART is configured to 57600 Baud rate)
Please find the below example command:
int Start_Command[8] = { 0x01, 0x03, 0x00, 0x00, 0x01, 0x01, 0xFE, 0xFB};
Start_Command :
0x01- Node address
0x03- Speed command
0x0000- Default value
0x0101 - Target speed 257 RPM
0xFBFE - Checksum ( -1 * ( 0x0301 + 0x0000 + ox 0101))
To get the reply from the Slave( iMotion) the baud rate must be configured correctly and the Motor command must be in a correct format.
Refer to section 2.3 ( User UART) for commands-https://www.infineon.com/dgdl/Infineon-MCESW-RM-UserManual-v01_03-EN.pdf?fileId=5546d462719b59230171...
Please let us know if you are able to start the motor by using the above command format.
Thanks,
Krupashankar