iMOTION™ - Controller, SmartDriver & SmartIPM

cancel
Showing results for 
Search instead for 
Did you mean: 
Ask a question

Recent discussions

Sort by:
AG_Serad
iMOTION™ - Controller, SmartDriver & SmartIPM
Hello I'm using script into IMC102T. I use a global variable which is read via serial communication. This variable is refreshed in Task1 via many line... Show More
AG_Serad
iMOTION™ - Controller, SmartDriver & SmartIPM
Hello, I'm using the IMC102T.   I configured to detect the AC under Voltage (180V) According the user manual, §2.2.2.3, it is say that in case of unde... Show More
User22403
iMOTION™ - Controller, SmartDriver & SmartIPM
I've recently started using the IMC099T in a new project, controlling a 24V BLDC motor.I am trying to get my microcontroller (ESP32) to communication ... Show More
User18018
iMOTION™ - Controller, SmartDriver & SmartIPM
Hi all, This is example Uart Command for IMC101-102T Example Uart Command for IMC101-102TPrecautions1- What is inconsistent with the current version o... Show More
n6xb
iMOTION™ - Controller, SmartDriver & SmartIPM
Using the IMD111 eval board, my motor runs fine when I load the default parameter file and default firmware file into the part. However, if I then go ... Show More
FedericaLorini
iMOTION™ - Controller, SmartDriver & SmartIPM
IMC301
Solved
Hi, I need to get in touch with someone able to identify and solve a problem occurred to an italian distribuiton MM customer with IMC301 and the Multi... Show More
User22853
iMOTION™ - Controller, SmartDriver & SmartIPM
Hello Team,Please let me know how to rotate the BLDC motor using sensored algorith.I have done the sensorless rotation. Need to switch to the sensored... Show More
StMao
iMOTION™ - Controller, SmartDriver & SmartIPM
Hello everyone. I am testing the drive and control of our own IPM motor using the evaluation board (EVAL-M1-IM828A) and control board (EVAL-M1-101T, I... Show More
User22102
iMOTION™ - Controller, SmartDriver & SmartIPM
HiI got different speed reading.MCE trace say 3,500 rpmIn actual, the stroboscope say 3,550 rpm. I rely on stroboscope as it has been already checked... Show More
AG_Serad
iMOTION™ - Controller, SmartDriver & SmartIPM
HelloI will start to evaluate the IMC102T-F064 with the evaluation boar which include a Seeger debbuger to communicate between IMC102T-F064 UART0 and ... Show More