IMC102T-F064 Setting up PFC

Announcements

From sunburn to sun earn – we’ve got the power! Watch our #poweringgreen videos now.

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob
Mahimc2020
Level 3
Level 3
25 sign-ins 10 questions asked 10 replies posted
Hi
Thank you very much for designing the IC controller IMC102T-F064.
I configured this IC to start the Motor with PFC using UART connection.
I have no problem starting the Motor, but when I put the input control on VSP, the Motor starts but the power factor correction (PFC) does not start.
How can I start control input mode VSP, both motor and power factor correction(PFC) in input mode?
Should the power factor correction(PFC) command be given in the script? (PFC_command=1)?
Thank you.
0 Likes
2 Replies
snget2
Moderator
Moderator
Moderator
5 sign-ins First like received 25 replies posted
Hello Mahdi1368,
There is no built-in logic to link VSP with the operation of PFC. One needs to write up some script code to make it happen for a given application.
Some pseudo code for example.
If command = 1
Then PFC_command=1
Else
PFC_command=0

Regard,
Sid
0 Likes
Mahimc2020
Level 3
Level 3
25 sign-ins 10 questions asked 10 replies posted
Thanks for reply 🙂
0 Likes