Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 113237 Discussions

  • 115997 Members

  • 72188 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
EC3336
MOTIX™ MCU
can I find relevant materials for the die temperature sensor of the IMC300? Has it been calibrated at the factory? What methods do we have... Show More
alan_a
USB superspeed peripherals
Hello. I'm planning to work with the CYUSB3KIT-003. Reading and following the Kit User Guide,  I am able to complete section 2.1 FX3 SDK Installation ... Show More
mrfrizzy
Wi-Fi Bluetooth for Linux
I have a RPi 3b which is running a software package that hasn't had updates in many years and does not run on newer kernels. The system keeps randomly... Show More
SaCh_4769556
GaN
Dear IFX,   EVAL_AUDAMP24 board has IRS20957 + 400V GaN (IGT40R070D1) and i wonder on 100V GaN connection. Do we need any circuit change on Gate on/of... Show More
IArizal
XMC™
Hello Infineon, My project requires using the SMIF (Octal SPI) to transfer from external flash memory into XMC7200 internal RAM through P-DMA. Based o... Show More
fafr_4822411
CAPSENSE™ & MagSense
HI   I would like to build a trigger control for a youtube maker project , using the TLE493D-W2B6 I have an TLE493DW2B6 shield2go board, and I connect... Show More
n19en
Switches (Magnetic sensors)

What is the magnetic hysteresis of the TLI5590 sensor? Does it differ on the two bridges?

MSS
PSoC™ 6
Hi, I am using CY8C6245LQI-S3D42 and I used the DFU examples to boot the system and created the application to run on AM4 core and everything is worki... Show More
jvavra_UICO
ModusToolbox™
I'm exploring the CSX Touchpad Tuning sample application using the PSoC4 MAX Pioneer kit. In the user manual for the CAPSENSE Tuner app, it says "The ... Show More
zanmarinsek
AURIX™
Hello, I'm working on a project for a company where I need to implement Ethernet with UDP using Lwip. I noticed that there is no example on this parti... Show More