Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 113335 Discussions

  • 116031 Members

  • 72228 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
Henrik
AURIX™
Lookin in the TC38x datasheet I find mention of buffer type per pin. Is there some more information available on what this means in detail? Or perhaps... Show More
kbeaskoetxea
Contactless power and sensing ICs
Hi support, I would like to set-up a UART connection on my NAC1080 using the GPIO0 and GPIO2 in order to communicate with my PC the messages that the ... Show More
Translation_Bot
AURIX™
The current TC397_TFT v1.0 development board uses the TC397 A step of the chip, but I see ADS are TC397 B step routines, I will ADS in a few examples ... Show More
Translation_Bot
TRAVEO™ T2G
Hello, everybody: I encountered the following problem, read the value in the register, check the register is "0x80000e23", but after reading, the firs... Show More
Translation_Bot
Radar sensor
I tried to configure it using the above code, but it reports an error at device.set_acquisition_sequence(sequence). Using the sample program found in... Show More
Wendy2
MOTIX™ MCU
大家好! 官方程序里的延时函数Delay_us(uint32 delay_time_us),在实际测试时,有个奇怪的现象。 测试程序看门狗设置1008ms,测试程序延时方式如下: Delay_us(500000); (void)WDT1_Service();     //延时500ms,喂狗 De... Show More
ContiShaw
AURIX™
This Q&A just discussed P/D Flash, AURIX™ MCU: Error Correction Code (ECC) support - KBA238244 My question: is there special ECC for  RAM and CAN rele... Show More
PrasadA
XMC™
Hello,I am trying to flash littlefs filesystem on thze qspi external serial flash memory in XMC7100 V1.1.As I see library mtb-littlefs is not included... Show More
DoJe_4634471
Radar sensor
Hi, I am new to radar sensors. To analyze radar data, I have plotted FIFO data read from BGT60TR13C in time domain. My concern is whether the data in ... Show More
Horizonxx
XMC™
Hello Can we allocate 2 nodes on MULTICAN_CONFIG_0, and operate all message objects of both the nodes using only one CAN_Rx and CAN_Tx through transce... Show More