Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 112802 Discussions

  • 115832 Members

  • 71848 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
hawkp
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
I have fast data >200Mbps to be sent out to a Wifi access point. The protocol of this fast data is SLVS.  So I would use an FPGA to convert from SLVS ... Show More
ETRO_SSN583
PSoC™ 5, 3 & 1
Trying to get the Phoenix RLC tester project up and running.   Cannot find the component project file.   Regards, Dana. Show More
ChRi_4627521
PSoC™ 6
Eclipse IDE for ModusToolbox Version: 2.2.0 Build ID: 2181 CY8CPROTO-062-4343W KitProg3 I've been developing code using FreeRTOS for several months no... Show More
glowingkitty
USB EZ-PD™ Type-C
I designed a PCB that uses the CYPD3177 for both negotiating 9V at 2A minumum and convert the voltage down to 5V via a buck converter, but which also ... Show More
Ziad
XMC™

Hello,

how could i flash the xmc4500 using the MiniProg4? Is it possible?

Thanks.

cfischang
Nor Flash
I'm currently investigating the S70FL01GSAG 1Gb device as a replacement for the S25FL512S 512Mb device due to a larger flash capacity requirement. Whi... Show More
Engin6
IGBT
Dear community members I need to measure the temperature of an FF800R12KE7 IGBT with an NTC sensor. I would like to know what is the best position to ... Show More
g_bigChungus
AURIX™
Hi there, Can you confirm whether the statement below is true? "Where a watchdog timeout alarm (CPU or safety) is triggered the microcontroller will a... Show More
Rajendra
AIROC™ Bluetooth
HI, We were testing the BLE functionality with Android9 OS. During testing we found that BLE connection failed with the error showing  "bt_smp : dhkey... Show More
kirankumar_infy
TRAVEO™ T2G
Hello Experts, I am referring this document (page 36) for my configuration of UART to 115200 baudrate. I am not getting desired output on my putty ter... Show More