Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 113760 Discussions

  • 116255 Members

  • 72596 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
TR932_XT
AURIX™
We have been working on debugging an issue where the TC29x Ethernet receiver halts after being saturated with messages and the Ethernet module must be... Show More
Iulian_C
Speed (Magnetic sensor)
Hi Everyone, Today we are manufacturing sensors using the assembly KMI15/1 manufactured by NXP. We need an alternative because KMI15/1 is obsolete. We... Show More
wmaxfield
PSoC™ 5, 3 & 1
I can program the psoc5 using openocd now, with some caveats. However, if an NVL entry exists, it stops. I have a project which somehow did something ... Show More
davisg84
MOSFET (Si/SiC)
I am working on a wireless charger for electric vehicles and need MOSFET modules for generating the high-frequency AC. The FF3MR20KM1H might fit our a... Show More
gkuhn88
PSoC™ 6
I am attempting to follow the "Secure Boot" SDK user guide but continually run into the same problem. When attempting to setup the "CySecureTools" wor... Show More
jnagy
USB superspeed peripherals
I am implementing a UVC MJPEG application using the FX3 which is sent MJPEG video frame data from an FPGA and we are seeing the following frame corrup... Show More
GrCa_1363456
USB superspeed peripherals
I plan to port my design from CY7C68013A to CYUSB2014. Can I use the same development tool and just select the different component? Are there any pote... Show More
John_Skeldon
AURIX™
i'm trying SPI_CPU_1_KIT_TC334_LK.. I've joined SPI_A to SPI_B (confirmed on schematic for dev kit - - i hope). when the code runs i dont have an LED ... Show More
GrCa_1363456
MOSFET (Si/SiC)
Where are CAD models for QDPack. There are .pdf files at https://www.infineon.com/cms/en/product/packages/PG-HDSOP/PG-HDSOP-22-1/ These are NOT CAD mo... Show More
RangoWang
Radar sensor
My radar is Distance2GoL. I reconfigure the firmware in config.h, make the one frame is 40ms,  each frame has 10 pulses, and each pulse lasts 2ms. Fir... Show More