Featured Discussions
text.format{('custom.tabs.no.results')}
Hii,
I'm using CYTVII-C-2D-6M-327-SET evaluation kit for my project. I require information's about pinout details exposed out in dev kit and its schematic diagram .
I couldn't get those documents. could you support on this ?
Thanks.
Show LessHello,
I am trying to understand the working of various peripherals for the TC397 board. I came across the IfxPort_reg.h file for GPIOs and noticed that there are some missing nos. in the port modules for example after MODULE_P00, MODULE_P01, and MODULE_P02, there is no MODULE_P03. It skips directly to MODULE_P10. More examples can be seen in the screenshot below. I am not sure if this is common knowledge, but is there any particular reason the port modules are named in such a way?
Thanks
Show Less
Hi,
For Aurix TC397 is there any RTOS/Software BSP available other than AUTOSAR 4.2
Thank you
Hi,
I am having the Traveo-T2G kit. CYTVII-2D-4M-216 set and the CYT3DLABHBES cpu.
I am running the TRAVEO T2G Sample driver Library provided by infineon. I want to use freeRTOS in the project.
Previously I was using IAR V9.30.1 , in that version I could see the option in workspace to switch to the RTOS supported workspace.
Now I am using IAR v8.22.2, here no option in workpace for RTOS. Can somebody help me to run RTOS example.
Show Less
置換え代替製品を御教示頂きたくお願い致します。
Maker:Torex Semicon
PN:XC3101AC70NR-G (Temperature Sensor)
Status:EOL
Cross Referenceでは、ヒットせず、御手数ですが、
アドバイス頂けますと幸いです。
宜しくお願い致します。
Show Less请问 cyusb3014 如何升级内部ROM 的 bootloader
您好
目前我们使用cyusb3014 这颗芯片,配置PMODE从SPI 启动;测试电源复位时序ok,PMODE配置ok,但是又概率SPI CK没有输出波形,启动异常,请问可能的原因