Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 113798 Discussions

  • 116271 Members

  • 72629 Solutions

filter icon

Featured Discussions

Sort by:
Filter by forum
DHTechMichael
Current (Magnetic sensor)
Hello There, I was looking for alternatives for DZ600N12K/DZ600N14K as both of them were EOL and it is tough to procure any of them in the market. Cou... Show More
Translation_Bot
AIROC™ Bluetooth
Hi,How can I burn a program into the 20829 board I drew? Can I use the J11 of 20829EVK to do it? Or is there any other burning tool?smartconx_target@Q... Show More
taegyunahn
TRAVEO™ T2G
Hi, I'm using CYT4BF. I confirmed that the Bandgap Reference circuits can be set to higher current mode or low power in the PWR_CTL2.BGREF_LPMODE regi... Show More
bwiese
PSoC™ 5, 3 & 1
Hi!I've grown an inherited mess into a now now-useful application running on PSOC 5LP (CY8C5868AXU-035), using PSOC Creator 4.4.We burn our board FW u... Show More
gkuhn88
PSoC™ 6
Hello,  As a result of the difficulties of ModusToolbox i have been attempting to use the Mbed Studio with the PSoC64 Wi-Fi BT Secure Boot Pioneer kit... Show More
kotnikyeah
Legacy microcontrollers
Hello everyone, I use MCU that has 3V3 output and 5V input tolerant pins, but for my application I need to have 5V output and 5V tolerant input pins. ... Show More
TOMMAT
Other Technologies General
Dear team   I would like to use the MA5302 to create a single-supply, single-ended input stereo amplifier. There was an evaluation board for MA5302 wi... Show More
Marcelo_Macedo1
AIROC™ Bluetooth
Hi, Can you please advise if the CYW20829B0-P4 module supports Zephyr? If not, is there any plan for that? Regards, Marcelo Macedo - FAE at Neutronics Show More
RichardLC68
AIROC™ Wi-Fi and Wi-Fi Bluetooth Combos
Hello, we ported the wifi stack in our new product, it has a WiFi stability issue, mainly it shows SDIO bus communication error, we made a restart sta... Show More
TR932_XT
AURIX™
We have been working on debugging an issue where the TC29x Ethernet receiver halts after being saturated with messages and the Ethernet module must be... Show More