Featured Discussions
I am currently working in a power bank power delivery project and got CYPD72721-68LQXQ USB C PD controller. My circuit board is small , so to show status such as LED indicators or charging status etc I do not want to use an additonal MCU to handle these things. Can I use CYPD72721-68LQXQ for that purpose too?
Hi,
When we compared samples of the CY8C4124AXI-443T produced at different dates and factories, the differences detailed below were detected.
In order to understand which of these differences in top marking and lead frames are correct, we need your official statements that we can use.
Reverse Logo colors, different alignment and size
TWNxxxx vs xxxx (There is no any Country Code. PHI or TWN)
Different Lead Frames (X-ray image)
Are there any official statements about these differences?
Show Less
你好,我在SDK:Slavefifo5bit的范例中想要加多一个线程去供我做其他的功能,可是我是用了threadcreate之后我的usb设备就无法初始化了,请问是怎么回事呢??
I am using Application Kit TC3X7 V2.0 TFT board
I have configured BMHD but the board all the time boots from Internal flash ignoring BMHD settings
If i want to use Alternate Boot Mode or BMI to boot , which all changes i need to do on the board?
Show LessHello,
We are trying to flash binaries which has empty cells using Infineon MemTool (version 4.08.01) after the P-Flash erased.
But the Memtool programing the empty cells with all zreo values.
SW is checking that area has in erased state or not. So, SW is not working b'coz empty cells have values all zeros.
but other debugger flashing working with option: program empty cells "FALSE" setting
Please help us. if any setting required to do in Memtool
Show LessHi,
I want to translate the following App Note to Japanese. Please confirm to my work.
"Application note - MOTIX TLE987x Motor Control FOC Demo"
URL: https://www.infineon.com/dgdl/Infineon-MOTIX_TLE987x_Motor_Control_FOC_Demo_App_Note-ApplicationNotes-v01_00-EN.pdf?fileId=8ac78c8c8929aa4d0189441becff46d3
This application is large and will be divided into three parts.
I would like to translate pages 1 through 26 in this case.
Best Regards,
Hayashi.K
Hello Community,
I am started using TC233 development board for few days and i ant now to display a hello wolrd or messga in the Console but i didn' found how to do i tried also to display it on the putty but also it doesn't work.
is there any code exmaple or something that can help me.
Thank you
I inherited a project which uses a quite old version of the GCC toolchain when opening the project I receive the error:
Unable to find the tool chain with name: "ARM CM3-GCC 4.2.1". Select a different tool chain for your workspace.
How do I change the toolchain version of the project? I tried finding this version on the ARM developer project. The oldest version that I could find is 4.6 2012q4. Can someone point me to where to change the project settings or provide a link to the old version of the toolchain?
Show LessDear All,
I use the DAVE ide v4 with the nano library, calling the SPI-MASTER-EnableSlaveSelectSignal() and SPI-MASTER-DisableSlaveSelectSignal() functions cannot raise or lower the CS pin of SPI. However, when sending data through SPI, when using an oscilloscope to check the status of SCL and MOSI pins, they generate waveforms that are normal, but the CS pin remains in a high level state.
Configure this CS pin as an IO port, manually pull up or down the CS pin, but use the BUSY flag in the TBUF register as the completion of sending. When pulling up the CS pin, there will be a situation where there is still one byte that has not been sent, but the CS pin has been pulled up.
What may be the reason why the two API functions generated by calling cannot control the CS pin state; How can I avoid manually raising or lowering the CS pin when there is still one byte of data not sent?
Thanks.
Show LessHello,
Please tell me how to use EVAL-1ED38x0DCT.
Even if you connect it to a PC via USB, the click start button will not appear and you will not be able to use it, as shown below.
Is there any solution?
best regards,
Show Less