Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

Welcome to the Infineon Developer Community

  • 113812 Discussions

  • 116283 Members

  • 72658 Solutions

filter icon

Featured Discussions

manish0834
AURIX™
Hello, I am trying to understand the working of various peripherals for the TC397 board. I came across the IfxPort_reg.h file for GPIOs and noticed th... Show More
Sri_Cy
AURIX™

Hi, 

For Aurix TC397 is there any RTOS/Software BSP available other than AUTOSAR 4.2

Thank you

Muniyappan
TRAVEO™ T2G
Hi,  I am having the Traveo-T2G kit. CYTVII-2D-4M-216 set and the CYT3DLABHBES  cpu. I am running the TRAVEO T2G Sample driver Library provided by inf... Show More
KOTO
Switches (Magnetic sensors)
置換え代替製品を御教示頂きたくお願い致します。 Maker:Torex Semicon  PN:XC3101AC70NR-G (Temperature Sensor) Status:EOL Cross Referenceでは、ヒットせず、御手数ですが、 アドバイス頂けますと幸いです。 宜しくお願い致... Show More
DHTechMichael
Current (Magnetic sensor)
Hello There, I was looking for alternatives for DZ600N12K/DZ600N14K as both of them were EOL and it is tough to procure any of them in the market. Cou... Show More
Translation_Bot
AIROC™ Bluetooth
Hi,How can I burn a program into the 20829 board I drew? Can I use the J11 of 20829EVK to do it? Or is there any other burning tool?smartconx_target@Q... Show More
taegyunahn
TRAVEO™ T2G
Hi, I'm using CYT4BF. I confirmed that the Bandgap Reference circuits can be set to higher current mode or low power in the PWR_CTL2.BGREF_LPMODE regi... Show More
bwiese
PSoC™ 5, 3 & 1
Hi!I've grown an inherited mess into a now now-useful application running on PSOC 5LP (CY8C5868AXU-035), using PSOC Creator 4.4.We burn our board FW u... Show More
gkuhn88
PSoC™ 6
Hello,  As a result of the difficulties of ModusToolbox i have been attempting to use the Mbed Studio with the PSoC64 Wi-Fi BT Secure Boot Pioneer kit... Show More
kotnikyeah
Legacy microcontrollers
Hello everyone, I use MCU that has 3V3 output and 5V input tolerant pins, but for my application I need to have 5V output and 5V tolerant input pins. ... Show More