- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Hi team,
We are facing an issue regarding changing an MCU from XMC1403Q040X0200AAXUMA1 to XMC4108Q48K64BAXUMA1.
In XMC1403Q040X0200AAXUMA1 , We have SPI chip select of 4 numbers. But in new XMC4108Q48K64BAXUMA1, We have only 2 chip select pins available as per XMC Pinout Tool and DAVE IDE. Can we use GPIO's as a Chip select pins?
XMC1403Q040X0200AAXUMA1 PIN OUT Tool
XMC4108Q48K64BAXUMA1 PIN OUT Tool
Solved! Go to Solution.
- Labels:
-
ispn:13708:1:0
-
l1:408:1:0
-
l2:485:1:0
-
l3:493:1:0
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1: If you use the device which offer 4 slave select signals which you need, you can config it directly.
2: If you want to use the xmc4108-48pin chip which don't have dedicated four SSC slave select signals, you can use the GPIO to control.
3: I don't think GPIO control is far better, but as you said, it can create the communication. You can set up a test project to test it.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
The XMC4108Q48K64BAXUMA1 SPI SS pin numbers can only be configured as 2. Because of the hardware restriction.
Your GPIO pins can't be used to act as the ss pin. But if you want to use the GPIO to emulate the SPI, it is another thing.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Thank you @LinglingG_46 for your response. We are not trying to emulate SPI but only changing CS pin since we have 4+ slaves sharing the same SPI. Normally in Controllers It's possible to implement the same. Can you explain in detail why it is not possible in XMC4108Q48K64BAXUMA1.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
XMC4108Q48K64BAXUMA only supports one CS (chip select) pin.
Just like the pinout tool, it has two choices, one is P0.7 and another is P1.0.
If you want to have 4 slaves, it is recommended that you can choose another part of device which support the feature.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
Once we give a low voltage at CS pin of any slave device, it enables the communication between master and Slave. GPIO could be far better for that operation right? What makes you to say only dedicated pin works?
We already have this part in bulk stock and would like to get a very detailed explanation from your Firmware experts too.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Report Inappropriate Content
1: If you use the device which offer 4 slave select signals which you need, you can config it directly.
2: If you want to use the xmc4108-48pin chip which don't have dedicated four SSC slave select signals, you can use the GPIO to control.
3: I don't think GPIO control is far better, but as you said, it can create the communication. You can set up a test project to test it.