Announcements

Help us improve the Power & Sensing Selection Guide. Share feedback

Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

paddyliu
XMC™
Dears. When I created APP SPI MASTER, I found that the page of parameters configured in SPI was not fully displayed. What is the reason? I used DAVE 4... Show More
mrnoone
XMC™
Hello everyone. I have written a code which uses SWD pins as GPIO, but the code does not work. My question is that Can we use SWD protocol pins (clock... Show More
William_Zion
XMC™
Dear support team,    Kind need you help to answer below two questons,thanks!  1. My xmc4300 work in 144Mhz frequence and need EtherCat communication,... Show More
Wellin
XMC™

Hi  

Do we have MPPT solar charge controller solution for reference?

thanks

simoneSirius
XMC™
Hello everyone, I'm trying to implement the profinet slave stack on xmc4700. On wireshark I see that the masters (Siemens PLC) sends a frame 60 bytes ... Show More
Lubrzz
XMC™
Hello, we are planning to use ADIN1200 PHY for ethercat slave based on XMC4300 Are there any source example how to manage ADIN1200 PHY ? We found a sc... Show More
Suraj
XMC™
Greetings of the day, Am presently working on XMC1300 control card and running BLDC motor using BLDC_SCALAR_HALL example code Am trying to read Phase ... Show More
Authur
XMC™
I'm using XMC4200 to drive a 400W PMSM motor, 48V DC voltage,  and uses V/F Start with transitoin to FOC at low speed operation(600RPM),  I able to ru... Show More
vouria
XMC™
Hello I’m using the KIT_XMC1X_AK_MOTOR and I believe I have two problems. I am using the BLDC_SCALER_CTRL APP and if I run the firmware using the Adap... Show More
gachetp
XMC™
Hello,  I use a XMC130T038 and I implement an I2C. When I'm in debug mode, my system starts but is blocked directly in I2C init.  I have the save pro... Show More