Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

Nichol
XMC™
It worked at first, but I couldn't connect it after debugging several times without changing BMI. The 'DBG'LED is On. I try some step are follows: 1.J... Show More
90670
XMC™
Hi everyone, I want to use my XMC4700 MCU to communicate with other module using SPI protocol (I want use USIC hardware in the MCU, I don't want to us... Show More
An_1
XMC™
Hi,  I am running two  Ether CAT boards simultaneously . I followed through XMC4800 Ether CAT One cycle Client2ClientCommunication document. In the do... Show More
MiroslavCZE
XMC™
Hello,I´m looking for best solution to start. I need to use one XMC4300 device in two modes: ethercat or ethernet (not together). Is it possible to ju... Show More
jameswbush
XMC™
Any example of reading 32-bit I2S PCM data with XMC4500 using DMA, which is how it is usually done in other MCUs like Microchip, Texas Instruments, ST... Show More
zhouqizhen
XMC™

下午好:

当我使用XMC闪光灯更新距离2Go的MCU程序时,我遇到了一个问题:

当我断开微型USB电缆与“调试”端口的连接并将其连接到“默认”端口时,PC无法识别串行端口。

我该怎么办?

谢谢!

jamesk
XMC™
I am calling SPI_MASTER_StartTransmitDMA() to transfer from memory to peripheral device. Host is XMC4700 and Peripheral is a radio device. I can sniff... Show More
zhouqizhen
XMC™
Good afternoon! When I used the XMC flash to update the MCU program for distance2Go, I had a problem. When I disconnect the micro-USB cable from the d... Show More
kalsi
XMC™
Hello team, Hope you are doing well. Question about ADC channels on XMC 4400. The XMC 4400 Reference manual mentions that we have 4 ADC blocks with 8 ... Show More
Suraj
XMC™
Hi Team Currently am working on 'Over Current Protection' in BLDC Hall sensor Controlling  using XMC1300 MCU with custom motor designed for max curren... Show More