Tip / Sign in to post questions, reply, level up, and achieve exciting badges. Know more

cross mob

XMC™ Forum Discussions

EXT-GuptaRak
XMC™

Is there any process to do the board hard reset  ?

SunshineQAQ
XMC™
Hi, Urgent, xmc7100 chip, in pwm dead zone mode how to achieve pwm channel output complementary channel output off, over 2s and then reverse. Best Reg... Show More
Translation_Bot
XMC™
     smartconx_target@Q!w2e3r4t5y6u7i8o9p0||/t5/XMC/XMC7000-%E5%8F%8C%E6%A0%B8%E7%9A%84M7-cpu%E6%9C%80%E5%A4%A7%E9%A2%91%E7%8E%87%E6%98%AF%E5%A4%9A%E... Show More
tsd
XMC™
请教: 1.我有一个xmc4300的ETHCAT_SSC_XMC43工程可以实现ethercat通信。 2.我还有一个xmc4400的BLDC_SCALAR_HALL_XMC44_uCProbe工程可以实现BLDC的驱动。 3.我现在想把BLDC_SCALAR_HALL_XMC44_uCProbe的... Show More
Alex8274
XMC™
Dears 当XMC1400 的供电超过了其最大工作电压,XMC1400的I/O 引脚会是什么状态?开路or GND? 会不会有确定的高电平输出状态? Thanks! Alex. Wang Show More
hxp123cn
XMC™
In the EVAL_3K3W_TP_PFC_SIC code, AC and DC IIR filters are used. How can we calculate the parameters and K value of this IIR?       Show More
tsd
XMC™
请教, 我想参照参照XMC4400的PMSM_FOC_EXAMPLE_XMC44的Demo,用xmc4300实现PMSM_FOC_EXAMPLE_XMC44这个Demo。 现在遇到了我在选Queue C的时候没有这个选项,附件看图。请问怎么可以选到Queue C呢。xmc4300没有Queue C这... Show More
User17303
XMC™

调试XMC4500 WinUSB功能时,连接USB到设备后,电脑设备管理器读取到Infineon WinUSB Device ,但是缺少驱动程序,英飞凌官网上没有找到相关的驱动安装包,特在此求助,能给个Infineon WinUSB驱动安装包,万分感谢!

tsd
XMC™
请教: XMC的DAVE APPs和XMC Lib工程代码可以混用吗
ziad-shaarawy
XMC™

Is there a Dave App function or XMC function available that enables the connection of two pins to each other?